TI BLE Stack API Documentation
2.03.03
|
Functions | |
bStatus_t | GAPRole_SetParameter (uint16_t param, uint8_t len, void *pValue) |
Set a GAP Role parameter. More... | |
bStatus_t | GAPRole_GetParameter (uint16_t param, void *pValue) |
Get a GAP Role parameter. More... | |
bStatus_t | GAPRole_StartDevice (gapRolesCBs_t *pAppCallbacks) |
Does the device initialization. Only call this function once. More... | |
bStatus_t | GAPRole_TerminateConnection (void) |
Terminates the existing connection. More... | |
bStatus_t | GAPRole_SendUpdateParam (uint16_t minConnInterval, uint16_t maxConnInterval, uint16_t latency, uint16_t connTimeout, uint8_t handleFailure) |
Update the parameters of an existing connection. More... | |
void | GAPRole_RegisterAppCBs (gapRolesParamUpdateCB_t *pParamUpdateCB) |
Register application's callbacks. More... | |
bStatus_t GAPRole_GetParameter | ( | uint16_t | param, |
void * | pValue | ||
) |
Get a GAP Role parameter.
NOTE: You can call this function with a GAP Parameter ID and it will get a GAP Parameter. GAP Parameters are defined in (gap.h). Also, the "pValue" field must point to a "uint16_t".
param | - Profile parameter ID: GAP Role Parameters |
pValue | - pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
void GAPRole_RegisterAppCBs | ( | gapRolesParamUpdateCB_t * | pParamUpdateCB | ) |
Register application's callbacks.
pParamUpdateCB | - pointer to param update callback. |
bStatus_t GAPRole_SendUpdateParam | ( | uint16_t | minConnInterval, |
uint16_t | maxConnInterval, | ||
uint16_t | latency, | ||
uint16_t | connTimeout, | ||
uint8_t | handleFailure | ||
) |
Update the parameters of an existing connection.
connInterval | - the new connection interval |
latency | - the new slave latency |
connTimeout | - the new timeout value |
handleFailure | - what to do if the update does not occur. Method may choose to terminate connection, try again, or take no action |
bStatus_t GAPRole_SetParameter | ( | uint16_t | param, |
uint8_t | len, | ||
void * | pValue | ||
) |
Set a GAP Role parameter.
NOTE: You can call this function with a GAP Parameter ID and it will set the GAP Parameter. GAP Parameters are defined in (gap.h). Also, the "len" field must be set to the size of a "uint16_t" and the "pValue" field must point to a "uint16_t".
param | - Profile parameter ID: GAP Role Parameters |
len | - length of data to write |
pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
bStatus_t GAPRole_StartDevice | ( | gapRolesCBs_t * | pAppCallbacks | ) |
Does the device initialization. Only call this function once.
pAppCallbacks | - pointer to application callbacks. |
bStatus_t GAPRole_TerminateConnection | ( | void | ) |
Terminates the existing connection.