Terms and Acronyms

BIM
Boot Image Manager, the software bootloader
CCA
CCFG
Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
CCS
Code Composer Studio
IAR
IAR Systems
MCU
Microcontroller Unit
OAD
Over the Air Download
OOB
Out-Of-Box
PIB
Personal-Area-Network Information Bases
RCFG
TI-RTOS in ROM Configuration Table
ROM
Read-only Memory
SNV
Simple Non-Volatile storage
ICALL
Indirect Call
RTOS
Real Time Operating System
FFD
Full Functionality Device
RFD
Reduced Functionality Device
CLI
Command Line Interface
GUI
Graphical User Interface

TI-RTOS Terms and Acronyms

Hwi
A TI-RTOS Hardware interrupt.
Idle Task
A TI-RTOS default task that is executes when no other higher priority thread needs to run.
RTC
Real-time Clock
Swi
A TI-RTOS Software interrupt.
TI-RTOS
Texas Instruments Real Time Operating System
Zero-Latency Interrupts
An interrupt when genereated, will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see this wiki article.

Over the Air Download (OAD) Terms and Acronyms

BIM
Boot Image Manager
OAD
Over the Air Download
OAD Client
The device whose firmware is being upgraded over the air. This is assumed to be a CC13xx device running the TI 15.4-Stack OAD service.
OAD Server
The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Client.

Sensor Controller Terms and Acronyms

SC
Sensor Controller
SCS
Sensor Controller Studio