Debugging¶
External Resources¶
- Debugging common application problems with TI-RTOS video presentation on training.ti.com.
Debug Interfaces¶
The CC13x0 platform supports the cJTAG (2-wire) and JTAG (4-wire) interfaces. Any debuggers that support cJTAG, like the TI XDS100v3 and XDS200, work natively. Others interfaces, like the IAR I-Jet and Segger J-Link, can only be used in JTAG mode but their drivers inject a cJTAG sequence which enables JTAG mode when connecting. The hardware resources included on the devices for debugging are listed as follows. Not all debugging functionality is available in all combinations of debugger and IDE.
- Breakpoint unit (FBP) – 6 instruction comparators, 2 literal comparators
- Data watchpoint unit (DWT) – 4 watchpoints on memory access
- Instrumentation Trace Module (ITM) – 32 × 32 bit stimulus registers
- Trace Port Interface Unit (TPIU) – serialization and time-stamping of DWT and ITM events
The SmartRF06 Board contains a XDS100v3 debug probe, and the CC2650 LaunchPad contains the XDS110 debug probe. These debuggers are used by default in the respective sample projects.
Connecting to the XDS Debugger¶
If only one debugger is attached, the IDE uses it automatically when you click the button in CCS.
If multiple debuggers are connected, you must choose the individual debugger to use. The following steps detail how to select a debugger in CCS.
Configuring Debugger in CCS¶
To select a specific debugger in CCS, do as follows:
Find Serial Number¶
To find the serial number for XDS100v3 debuggers, do as follows.
- Open a command prompt.
- Run
C:\ti\ccsv7\ccs_base\common\uscif\xds100serial.exe
to get a list of serial numbers of the connected debuggers.
For XDS110 debuggers (Launchpads), run the following command:
c:\ti\ccsv7\ccs_base\common\uscif\xds110\xdsdfu.exe -e
Configure serial number¶
|
|
|
|
|
|
|
Breakpoints¶
CCS reserves one of the instruction comparators for stepping etc. Five hardware breakpoints are available for debugging. This section describes setting breakpoints in CCS.
Breakpoints in CCS¶
To toggle a breakpoint, do any of the following.
- Double-click the area to the left of the line number.
- Press Ctrl+Shift+B.
- Right-click on the line.
A breakpoint set on line 207 looks like the following.
For an overview of the active and inactive breakpoints, click on View –> Breakpoints.
To set a conditional break, do as follows.
- Right-click the breakpoint in the overview.
- Choose Properties.
When debugging, Skip Count and Condition can help skip a number of breaks or only break if a variable is a certain value.
Note
Conditional breaks require a debugger response and may halt the processor long enough to break an active RF connection, or otherwise disrupt timing on the debug target.
Considerations on Breakpoints¶
Breakpoints and Timing¶
Synchronous RF protocols like the Bluetooth low energy protocol are timing sensitive, and breakpoints can easily halt the execution long enough to lose network timing and break the link.
To still be able to debug, place breakpoints as close as possible to where the relevant debug information can be read or step through the relevant code segment to debug.
After you hit a breakpoint and read out the necessary debug information, it is recommended that you reset the device and re-establish the connection.
Breakpoints and Optimization¶
When compiler optimizations are enabled, toggling a breakpoint on a line of C code may not result in the expected behavior. Some examples include the following.
- Code is removed or not compiled in
- Toggling a breakpoint in the IDE results in a breakpoint some other unintended place and not on the selected line. Some IDEs disable breakpoints on nonexisting code.
- Code block is part of a common subexpression
- For example, a breakpoint might toggle inside a function called from one other function, but can also break due to a call from another unintended function.
- An if clause is represented by a conditional branch in assembly
- A breakpoint inside an if clause always breaks on the conditional statement, even if not executed.
TI recommends selecting an optimization level as low as possible when debugging. See Optimizations for information on modifying optimization levels.
Watching Variables and Registers¶
CCS provides several ways of viewing the state of a halted program. Global variables are statically placed during link-time and can end up anywhere in the RAM available to the project or potentially in flash if they are declared as a constant value. These variables can be accessed at any time through the Watch and Expression windows.
Unless removed due to optimizations, global variables are always available in these views. Local variables or variables that are only valid inside a limited scope are placed on the stack of the active task. Such variables can also be viewed with the Watch or Expression views, but can also be automatically displayed when breaking or stepping through code. To view the variables through CCS, do as follows.
Variables in CCS¶
You can view Global Variables by doing either of the following.
- Select View –> Expressions
- Select a variable name in code.
- Right-click and select Add Watch Expression.
- Select View –> Variables to
auto-variables
that are present at the current location when stepping through code.
Considerations When Viewing Variables¶
Local variables are often placed in CPU registers and not on the stack. These variables also have a limited lifetime even within the scope in which they are valid, depending on the optimization performed. CCS may struggle to show a particular variable due to its limited lifetime. The solution when debugging is as follows.
- Move the variable to global scope, so it remains accessible in RAM.
- Make the variable volatile, so the compiler doesn’t place the value in a register.
- Make a shadow copy of the variable that is global and volatile.
Memory Watchpoints¶
The DWT module contains four memory watchpoints that allow breakpoints on memory access. The hardware match functionality looks only at the address. If intended for use on a variable, the variable must be global. Using watchpoints is described for CCS as follows.
Note
If a data watchpoint with value match is used, two of the four watchpoints are used.
Watchpoints in CCS¶
- Right-click on a global variable.
- Select Breakpoint –> Hardware Watchpoint
- Go to the list of breakpoints (View –> Breakpoints)
- Right-click and edit the Breakpoint Properties to configure the watchpoint.
This example configuration ensures that if 0x42 is written to the memory location for Characteristic 1 in the Bluetooth low energy simple_peripheral example project the device halts execution.
TI-RTOS Object Viewer¶
CCS includes the RTOS Object Viewer (ROV) plug-in that provides insight into the current state of TI-RTOS, including task states, stacks, and so forth.
To access the ROV in CCS:
- Click the Tools menu.
- Click RTOS Object View (ROV).
This section discusses some ROV views useful for debugging and profiling. More details can be found in the TI-RTOS User’s Guide, including documentation on how to add log events to application code.
Scanning the BIOS for Errors¶
The BIOS Scan for errors view goes through the available ROV modules and reports on errors. This functionality can be a good point to start if anything has gone wrong. This scan only shows errors related to TI-RTOS modules and only the errors it can catch.
Viewing the State of Each Task¶
The Task Detailed view is useful for seeing the state of each task and its related runtime stack usage. This example shows the state the first time the user-thread is called. Figure 89. shows the Bluetooth low energy stack task, represented by its ICall proxy, the Idle task, the simple_peripheral task and the GAPRole task.
The following list explains the column in Figure 89.
- address
- This column shows the memory location of the Task_Struct instance for each task.
- priority
- This column shows the TI-RTOS priority for the task.
- mode
- This column shows the current state of the task.
- fxn
- This column shows the name of the entry function of the task.
- arg0, arg1
- These columns show abitrary values that can be given to entry function of the task. In the image, the ICall_taskEntry is given 0xb001, which is the flash location of the entry function of the RF stack image and 0x20003a30 (the location of bleUserCfg_t user0Cfg, defined in main()).
- stackPeak
- This column shows the maximum run-time stack memory used based on watermark in RAM, where the stacks are prefilled with 0xBE and there is a sentinel word at the end of the run-time stack.
Note
Function calls may push the stack pointer out of the run-time stack, but not actually write to the entire area. A stack peak near stackSize but not exceeding it may indicate stack overflow.
- stackSize
- This column shows the size of the runtime stack, configured when instantiating a task.
- stackBase
- This column shows the logical top of the runtime stack of the task (usage starts at stackBase + stackSize and grows down to this address).
Viewing the System Stack¶
The Hwi –> Module view allows profiling of the system stack used during boot or for main(), Hwi execution, and SWI execution. See System Stack for more information on the system stack.
The hwiStackPeak, hwiStackSize, and hwiStackBase can be used to check for system stack overflow.
Using the Memory Browser¶
CCS is able to show a representation of the memory on the device. In CCS you can index by address or by symbol name. As an example, consider the stack that was overrun in Figure 89.:
Simple Peripheral Task’s stack. Note BE watermark |
GAPRole Task’s stack. Note it’s completely filled. |
The solution in this case would be to increase the stack size for the failing task,
and see what the stack peak really is. The stackPeak
reported is relying on
how many watermark bytes are overwritten, so it can’t know how much the overrun
amounts to.
Because stacks are utilized from higher addresses towards lower addressed (upwards in the picture), stacks that overrun will tend to overwrite data at locations immediately before the stack.
Profiling the ICall Heap Manager (heapmgr.h)¶
As described in Dynamic Memory Allocation, the ICall Heap Manager and its heap are used to allocate messages between the Bluetooth low energy stack task and the application task and as dynamic memory allocations in the tasks.
Profiling functionality is provided for the ICall heap but is not
enabled by default. Therefore, it must be compiled in by adding
HEAPMGR_METRICS
to the defined preprocessor symbols. This
functionality is useful for finding potential sources for
unexplained behavior and to optimize the size of the heap. When
HEAPMGR_METRICS
is defined, the variables and functions listed as
follows become available. Global variables:
- heapmgrBlkMax
- The maximum amount of simultaneous allocated blocks
- heapmgrBlkCnt
- The current amount of allocated blocks
- heapmgrBlkFree
- The current amount of free blocks
- heapmgrMemAlo
- The current total memory allocated in bytes
- heapmgrMemMax
- The maximum amount of simultaneous allocated memory in blocks (this value must not exceed the size of the heap)
- heapmgrMemUb
- The furthest memory location of an allocated block, measured as an offset from the start of the heap
- heapmgrMemFail
- The amount of memory allocation failure (instances
where
ICall_malloc()
has returned NULL)
Functions¶
void ICall_heapGetMetrics(u16 *pBlkMax, u16 *pBlkCnt, u16 *pBlkFree, u16 *pMemAlo, u16 *pMemMax, u16 *pMemUb)
- Returns the previously described variables in the pointers passed in as parameters
int heapmgrSanityCheck(void)
- Returns 0 if the heap is ok; otherwise, returns a nonzero (that is, an array access has overwritten a header in the heap)
Determining the Auto Heap Size¶
The following procedure can be used to view the size of the ICall
heap when the auto heap size feature is enabled (HEAPMGR_SIZE=0
).
At runtime, view the value of the global memory symbol HEAPMGR_SIZE
after ICall_init()
has been executed in main(). The value of
HEAPMGR_SIZE
is the total size of the ICall heap. See
HEAPMGR_INIT()
in heapmgr.h for the source code implementation.
- In CCS Debug Session: View -> Expressions, add
HEAPMGR_SIZE
Note
The auto heap size feature does not determine the amount of heap needed for the application. The system designer must ensure that the heap has the required space to meet the application’s runtime memory requirements.
Due to memory placement, the actual heap size may be up to 4 bytes less.
To calculate the size of the ICall heap by inspecting the application map file in CCS:
The size of the heap is determined by the heapStart and heapEnd
global symbol addresses which are emitted by the linker. For example, the
simple_peripheral_cc2650lp_app.map
file:
20003f48 heapEnd
20001cc1 heapStart
The size of the ICall heap in this example is defined as:
0x20003f48 - 0x20001cc1 = 0x2287
or 8839 bytes
for the heap.
Optimizations¶
While debugging, turn off or lower optimizations to ease single-stepping through code. Optimization level can be configured at the project, file and function levels.
Project-Wide Optimizations¶
For debugging, ideally, the project-wide settings for optimization should be as low as possible. There may not be enough available space on the target to do this, but lowering just a couple of levels can be helpful.
In CCS
Project Properties –> CCS Build –> ARM Compiler –> Optimization
Single-File Optimizations¶
Note
Do single-file optimizations with care because this also overrides the project-wide preprocessor symbols.
In CCS
- Right-click on the file in the Workspace pane.
- Choose Properties.
- Change the optimization level of the file using the same menu in the CCS project-wide optimization menu.
Single-Function Optimizations¶
Using compiler directives, you can control the optimization level of a single function.
In CCS
#pragma FUNCTION_OPTIONS(myFunction, "--opt_level=0")
static void myFunction(int number)
{
// ...
return yourFunction(other_number);
}
Loading TI-RTOS in ROM Symbols¶
Some of the TI-RTOS kernel modules are included in ROM, and executed from ROM in order to save Flash space for the application. This can lead to some confusion, when only addresses are shown in the disassembly view and the call-stack view.
All TI-RTOS kernel code in ROM starts with address 0x1001xxxx
. In order to
make sense of the ROM’ed code, you need to include the symbol files in your
debug session.
In CCS
- While in debug mode, click the drop-down button next to the Load Program icon
- Select Add Symbols..
- Select Browse.. and find
<SDK\_INSTALL\_DIR>\kernel\tirtos\packages\ti\sysbios\rom\cortexm\cc26xx\r2\golden\CC26xx\rtos_rom.xem3
Deciphering CPU Exceptions¶
Several possible exception causes exist. If an exception is caught, an exception handler function can be called. Depending on the project settings, this handler may be a default handler in ROM, which is just an infinite loop or a custom function called from this default handler instead of a loop.
When an exception occurs, the exception may be caught and halted in debug mode immediately, depending on the debugger. If the execution halted manually later through the Break debugger, it is then stopped within the exception handler loop.
Exception Cause¶
With the default setup using TI-RTOS, the exception cause can be found in the System Control Space register group (CPU_SCS) in the register CFSR (Configurable Fault Status Register). The ARM Cortex-M3 User Guide describes this register. Most exception causes fall into the following three categories.
- Stack overflow or corruption leads to arbitrary code execution.
- Almost any exception is possible.
- A NULL pointer has been dereferenced and written to.
- Typically (IM)PRECISERR exceptions
- A peripheral module (like UART, Timer, and so forth) is accessed
without being powered.
- Typically (IM)PRECISERR exceptions
The CFSR
register is available in View –> Registers in CCS.
When an access violation occurs, the exception type is IMPRECISERR because writes to flash and peripheral memory regions are mostly buffered writes.
If the CFSR:BFARVALID flag is set when the exception occurs (typical for PRECISERR), the BFAR register in CPU_SCS can be read out to find which memory address caused the exception.
If the exception is IMPRECISERR, PRECISERR can be forced by manually disabling buffered writes. Set [CPU_SCS:ACTRL:DISDEFWBUF] to 1, by either manually setting the bit in the register view in CCS or by including <hw_cpu_scs.h> from Driverlib and calling the following.
#include <ti/devices/cc26x0r2/inc/hw_cpu_scs.h>
//..
int main()
{
// Disable write-buffering. Note that this negatively affect performance.
HWREG(CPU_SCS_BASE + CPU_SCS_O_ACTLR) = CPU_SCS_ACTLR_DISDEFWBUF;
// ..
}
Using TI-RTOS and ROV to Parse Exceptions¶
To enable exception decoding in the RTOS Object View (ROV) without using too much memory, use the Minimal exception handler in TI-RTOS. The default choice in the TI 15.4-Stack projects is to use no exception handler.
To set this up, change the section of the TI-RTOS configuration file that relates to M3Hwi so that it looks like the code below:
//m3Hwi.enableException = true;
m3Hwi.enableException = false;
//m3Hwi.excHandlerFunc = null;
m3Hwi.excHookFunc = "&execHandlerHook";
Then, make a function somewhere with the signature
void (*Hwi_ExceptionHookFuncPtr)(Hwi_ExcContext*);
such as the one below:
#include <ti/sysbios/family/arm/m3/Hwi.h>
// ...
volatile uintptr_t *excPC = 0;
volatile uintptr_t *excCaller = 0;
// ...
void execHandlerHook(Hwi_ExcContext *ctx)
{
excPC = ctx->pc; // Program counter where exception occurred
excCaller = ctx->lr; // Link Register when exception occurred
while(2);
}
Setting m3Hwi.enableException
to false enables the minimal handler,
which fills out the global Hwi_ExcContext structure that the ROV
looks at to show the decoded exception. By setting up an
excHookFunc, the minimal exception handler will call this function
and pass along a pointer to the exception context for the user to
work with. This structure is defined in
<ti/sysbios/family/arm/m3/Hwi.h>
.
When an exception occurs, the device should end up in that infinite loop. Inspect the ROV -> Hwi -> Exception information.
In this case, a bus fault was forced in the function writeToAddress by dereferencing address 0x0013 and trying to write to it:
void writeToAddress(uintptr_t *addr, int val)
{
*(int *)addr = val;
}
// ..
void taskFxn(...)
{
// ..
writeToAddress( (void*)19, 4 ); // Randomly chosen values
}
The write instruction was placed on line 79 of application.c, as indicated. To get a precise location, the write buffer was disabled as described earlier.
It can be instructive to look at the disassembly view for the locations specified by PC (program counter) and LR (link register). PC is the presumed exception location, and LR is normally the location the failing function should have returned to. As an example, the PC at this exception:
Some forensics is required here. We have from the Hwi decoding in ROV (and from
the exception context in the exception hook) that the program counter was
0x708e
when the exception occurred.
At that location there is a store instruction str r0, [r1]
meaning, store
the value in R0 to the memory address in R1. The business with SP
in the
figure above is related to optimization being turned off, so all local variables
are stored on the stack, even though in this case R0 and R1 could have been used
directly from the caller.
Now we know that the exception occured because soneone called writeToAddress with an invalid address.
Thanks to the exception decoder we can easily find the call site by
looking at the call stack, but if the call stack isn’t helpful, we can look
at lr
, which is seen in the exception decoder to be 0x198f
We can see here that R0 and R1 are initialized with constants. This means that some programmer has intentionally called the write function with an address that causes a busfault.
Most often the reason for a bus-fault is that a pointer is not initialized
and a function like writeToAddress
gets the pointer, assumes it’s valid and
dereferences the pointer and writes to the invalid address.
Debugging Memory Problems¶
This section describes how to debug a situation where the program runs out of memory, either on the heap or on the runtime stack for the individual thread contexts. Exceeding array bounds or dynamically allocating too little memory for a structure corrupts the memory and can cause an exception like INVPC, INVSTATE, IBUSERR to appear in the CFSR register.
Task and System Stack Overflow¶
If an overflow on the runtime stack of the task or the system stack occurs (as found using the ROV plug-in), perform the following steps.
- Note the current size of the runtime stack of each task.
- Increase by a few 100 bytes as described in Initializing a Task and System Stack
- Reduce the runtime stack sizes so that they are larger than their respective stackPeaks to save some memory.
Dynamic Allocation Errors¶
Profiling the ICall Heap Manager (heapmgr.h) describes how to use the ICall Heap profiling functionality. To check if dynamic allocation errors occurred, do as follows:
- Check whether
heapmgrMemAlo
orheapmgrMemAlo
are close toHEAPMGR_SIZE
- Check memFail to see if allocation failures have occurred.
- Call the sanity check function.
If the heap is sane but there are allocation errors, increase
HEAPMGR_SIZE
and see if the problem persists.
You can set a breakpoint in heapmgr.h in HEAPMGR_MALLOC() on the line hdr = NULL; to find an allocation that is failing.
To disable a symbol, put an x in front of the name. To disable power management, change POWER_SAVING to xPOWER_SAVING.
Options¶
Table 23. lists the preprocessor symbols used by the application in the simple_peripheral project. Symbols that must remain unmodified are marked with an N in the Modify column while modifiable; configurable symbols are marked with a Y.
Preprocessor Symbol | Description | Modify |
---|---|---|
USE_ICALL | Required to use ICall Bluetooth low energy and primitive services. | N |
POWER_SAVING | Power management is enabled when defined, and disabled when not defined. Requires same option in stack project. | Y |
HEAPMGR_SIZE=0 | Defines the size in bytes of the ICall heap. Memory is allocated in .bss section. When zero, the heap is auto sized. See Dynamic Memory Allocation | Y |
ICALL_MAX_NUM_TASKS=3 | Defines the number of ICall aware tasks. Modify only if adding a new TI-RTOS task that uses ICall services. | Y |
ICALL_MAX_NUM_ENTITIES=6 | Defines maximum number of entities that use ICall, including service entities and application entities. Modify only if adding a new TI-RTOS task that uses ICall services. | Y |
Display_DISABLE_ALL | All Display statements are removed and no display operations will take place. See Display.h for more details found in the Drivers virtual folder in the project. | Y |
BOARD_DISPLAY_EXCLUDE_UART | Define this symbol to exclude the UART used in the display driver. | Y |
BOARD_DISPLAY_EXCLUDE_LCD | Define this symbol to exclude the LCD used in the display driver. | Y |
MAX_NUM_BLE_CONNS=1 | This is the maximum number of simultaneous Bluetooth low energy collections allowed. Adding more connections uses more RAM and may require increasing HEAPMGR_SIZE. Profile heap usage accordingly. | Y |
CC26XX | This selects the chipset. | N |
<Board_Type> | In SimpleLink CC13x0 SDK, only CC2640R2_LAUNCHXL is supported. | N |
xdc_runtime_Assert_DISABLE_ALL | Disables XDC run-time assert | N |
xdc_runtime_Log_DISABLE_ALL | Disables XDC run-time logging | N |
HEAPMGR_METRICS | Enables collection of ICall heap metrics. See Dynamic Memory Allocation for details on how to profile heap usage. | Y |
Table 24. lists the only stack preprocessor options that may be modified:
Preprocessor Symbol | Description | Modify |
---|---|---|
POWER_SAVING | Power management is enabled when | Y |
defined, and disabled when not defined. Requires the same option in application project. | ||
GATT_NO_CLIENT | When defined, the GATT client is not included to save flash. GATT client is excluded from most peripheral projects, included in central and certain peripheral projects (for example, TimeApp). | Y |
BLE_NO_SECURITY | Unlink security functions from the dispatcher, used in conjunction with disabling GAP bond manager and SNV to further reduce flash space. | Y |
OSAL_SNV=1 | Select the number of NV pages to use for SNV. Each page is 4kB of flash. A minimum of one page is required when GAP_BOND_MANAGER is defined. See Using Nonvolatile Memory | Y |
OSAL_MAX_NUM_PROXY_TASKS=2 | Number of ICall-aware tasks the protocol task can communicate with. Default is 2. Increase this value if more RTOS tasks are added that make ICall protocol stack API calls. | Y |
EXT_HAL_ASSERT | Extended assert enables support for application callback for asserts. | Y |
Check System Flash and RAM Usage With Map File¶
Both application and stack projects produce a map file which can be used to compute the combined flash and RAM system memory usage. Both projects have their own memory space and both map files must be analyzed to determine the total system memory usage. The map file is in the output folder of the respective project. To compute the total memory usage, do as follows.
- Open the application map file (that is, simple_peripheral_cc2650r2lp_app.map).
Note
At the end of the file, three lines contain a breakdown of memory usage for read-only code, read-only data, and read/write data.
- Add the two values for read-only code and read-only data memory.
Note
This sum is the total flash memory usage for the application project. The read/write data memory is the total RAM usage by the application project.
- Note these values.
- Open the stack map file.
- Compute the same flash and RAM values for the stack project.
- Add the total flash memory value from the application with the total flash usage of the stack to determine the total system flash usage.
- Add the total RAM usage from the application with the stack to get the total system RAM usage.
For CCS, the map file of the respective project gives a summary of flash and RAM usage. To determine the remaining available memory for each project, see Flash and Memory Management (RAM). Due to section placement and alignment requirements, some remaining memory may be unavailable. The map file memory usage is valid only if the project builds and links successfully.