2. Release Specific¶
2.1. Processor SDK Android Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Android provides a fundamental software platform for development, deployment and execution of Android based applications and includes the following:
- Bootloaders & Filesystems
- SDK Installer
- Setup Scripts
- Makefiles
- eMMC Images
- Android UI
- Example Applications
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Android GPLv3 Disclaimer
2.1.3. Documentation¶
- Software Developer Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Android release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Getting Started Guide: provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs
. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 05.01.00¶
Released October 2018
What’s New
This is an “O-Pastry” based release of Processor SDK Android for AM57x.
Release Features
Following new features are enabled/tested in this release:
- Boot: fastboot, emmc boot, GP with FIT model
- Platform: LPAE support, SELinux Permissive mode
- Connectivity: USB2.0/USB3.0 Host, Gadget, Ethernet, SD card detect, eMMC
- Power: AVS0, MPU DVFS, ABB
- Thermal: Governors implemented for MPU (On Die), Monitoring implemented for all on chip sensors
- Video: 720p30 MP4/H264/MP2
- Audio: MP3/AAC playback
- Display: SGX accelerated UI and touch, DRM/KMS
SDK Components and Versions
Component | Version |
---|---|
Linux Kernel | 4.14.67 |
U-boot | 2018.01 |
Android | Android O-Pastry 8.1 |
Toolchain | Linaro GCC 7.2-2017.11 |
2.1.5. Supported Platforms¶
See Processor_SDK_Supported_Platforms_and_Versions for a list of supported platforms and links to more information.
2.1.6. Issue Tracker¶
2.1.6.1. Issues opened in previous releases that were closed on this release¶
Record ID | Platform | Title |
---|---|---|
LCPD-12486 | am57xx-evm | Android: libdrm-modetest not found in builds |
LCPD-12487 | am574x-idk, am57xx-evm | Android: eth port issue |
LCPD-12488 | am57xx-evm | Android: GFX warning seen on console |
LCPD-12512 | am57xx-evm | Board is not able to boot from emmc after flashing |
LCPD-12659 | am57xx-evm | Artifact observed during video decode operations |
LCPD-12679 | am574x-idk, am57xx-evm, am57xx-beagle-x15 | PVR_K: dmabuf error during video playback |
LCPD-12776 | am57xx-evm | Android: Graphics Error with Vellamo3 Benchmark |
LCPD-12782 | am571x-idk, am572x-idk | Android: AM571/572 IDK Board is not able to boot |
LCPD-12796 | am571x-idk, am572x-idk, am574x-idk, am57xx-beagle-x15 | Board requires USB input device to boot |
LCPD-12919 | am57xx-evm | PVR error observed during long term decode operations |
LCPD-12934 | am57xx-evm | Android: Robustness test: monkey fails |
LCPD-12935 | am571x-idk, am572x-idk, am574x-idk | PVR Dmabuf error observed |
LCPD-12938 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | GFXBench is not able to run no space left on device |
LCPD-13003 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | Need LCD detection logic for the IDK boards in the fastboot.sh script |
LCPD-13005 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | Component Test: POWERMGR_S_FUNC_CPUFREQ_BASIC Failed |
LCPD-13006 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | Seeing gadget disconnect/reconnect over and over ~5 minutes after booting |
LCPD-13009 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15 | AM57xx-IDK: Video played on LCD has long pauses when Android is booted without HDMI connected |
LCPD-13016 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | u-boot version being used is showing MMC fail messages |
LCPD-13467 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm | Services problems reported after reboot |
2.1.6.2. Issues found and closed on this release that may be applicable to prior releases¶
Record ID | Platform | Title |
---|---|---|
LCPD-13147 | am57xx-evm, am57xx-beagle-x15 | Regression to boot to UI with DB 178 |
LCPD-13568 | am571x-idk, am572x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15 | Android Boot failure due to binder errors |
LCPD-13601 | am571x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15 | Android: Treble: Gatekeeper service crash |
LCPD-13668 | am57xx-evm | Android: AM57x with LCD: Android System Internal error reported at boot_complete |
2.1.6.3. Known Issues¶
Record ID | Platform | Title | Workaround |
---|---|---|---|
LCPD-12491 | am57xx-evm | Android: Selinux warnings during bootup | |
LCPD-12511 | am57xx-evm | Audio record is not working | |
LCPD-12513 | am57xx-evm | Android O: Board takes longer to boot compared to MM | |
LCPD-12928 | am57xx-evm | Periodic frame freezes observed while decoding H264 video | |
LCPD-13409 | am571x-idk, am572x-idk, am574x-idk | Android: IDK: Bootloader images fail to boot from eMMC | |
LCPD-13602 | am571x-idk, am574x-idk, am57xx-evm, am57xx-beagle-x15 | Android: Treble: Selinux warnings and enforcing mode errors | |
LCPD-13723 | [android] allmodconfig fails to build on kernel build redirect | ||
LCPD-13795 | am571x-idk, am57xx-evm, am57xx-beagle-x15 | Android: Graphics service failure with “stop” and “start” command | |
LCPD-13796 | am57xx-evm | Android: monkey test causes system crash after 10 mins of execution | |
LCPD-13797 | am57xx-evm | Android:CTS Failures |
2.1.7. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup up your Android development environment, install the SDK and start your development.
2.1.8. Host Support¶
The Processor SDK is developed, built and verified on Ubuntu 14.04.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines
2.2. Supported Platforms and Versions¶
Supported Host Operating Systems
The following operating systems have been validated to work with our SDK.
- Linux SDK
Operating System | Version
|
Ubuntu | 14.04 (64-bit)
16.04 (64-bit)
18.04 (64-bit)
|
- RTOS SDK
Operating System | Version
|
Windows | 7 (64-bit)
|
Ubuntu | 14.04 (64-bit)
16.04 (64-bit)
|
- Android SDK
Operating System | Version
|
Ubuntu | 14.04 (64-bit)
|
Supported Platforms and EVMs
The following platforms and EVMs are supported with Processor SDK
2.3. Migration Guide¶
Overview
This page covers migration information for applications built on top of the Processor SDK for Android.
Processor SDK Android 05.01.00
- This is a maintenance update release of Processor SDK Android for AM57xx with Oreo. More details about Oreo can be obtained from here
- Multimedia with hardware acceleration is not supported
- Video decoding up to 720p resolution
- See 05.01.00 Release Notes for full list of modifications.
Processor SDK Android 05.00.00
- Linux Kernel and U-boot are updated to v4.14 and 2018.01 respectively, while the pastry continues to be Android-Oreo
- More details about Oreo can be obtained from here
- SD card creation now creates boot partition only with MLO, u-boot.img, and uEnv.txt. After flashing the eMMC device by Running Setup Scripts, SD card is required to boot AM57x IDKs. Keep the SD card plugged in, power cycle AM57x IDKs to use MLO and u-boot.img from the SD card and the rest from the eMMC. For AM57x GP EVM, SD card can be removed before the power cycle to boot Android with everything from the eMMC.
- VPE is not supported
- See 05.00.00 Release Notes for full list of modifications.
Processor SDK Android 04.03.00
- This is a maintenance update release of Processor SDK Android for AM57xx with Oreo. More details about Oreo can be obtained from here
- See 04.03.00 Release Notes for full list of modifications.
Processor SDK Android 04.02.00
- This is the first release of the Processor SDK Android for AM57xx with Oreo. Both U-Boot and Android Kernel are the same LTS as prior Processor SDK releases, i.e. 2016.05 and 4.4 respectively.
- More details about Oreo can be obtained from here
- See 04.02.00 Release Notes for full list of modifications.
Processor SDK Android 04.01.00
- This is the final release of the Processor SDK Android for AM57xx with Marshmallow. The next release will be based on Oreo
- See 04.01.00 Release Notes for full list of modifications.
Processor SDK Android 04.00.00
- This is the first release of the Processor SDK Android which supports AM57xx devices.
- See 04.00.00 Release Notes for full list of modifications.