MSP430UltrasonicLibrary
02_20_00_16
|
This structure is passed to USS_calculateOffsets API and calibration test result will be returned in this structure. More...
#include <ussSwLib.h>
Data Fields | |
float | upsAbsToFOffset |
float | dnsAbsToFOffset |
float | dToFOffset |
This structure is passed to USS_calculateOffsets API and calibration test result will be returned in this structure.
float _USS_dTof_absTof_offset_results_::upsAbsToFOffset |
Contains the averaged Abstof computation for UPS channel if USS_calculateOffsets API return USS_message_code_no_error and USS_dTof_absTof_offset_test_config.isCalculateUpsAbsTofOffset is set to true
Referenced by USS_calculateOffsets().
float _USS_dTof_absTof_offset_results_::dnsAbsToFOffset |
Contains the averaged Abstof computation for DNS channel if USS_calculateOffsets API return USS_message_code_no_error and USS_dTof_absTof_offset_test_config.isCalculateDnsAbsTofOffset is set to true
Referenced by USS_calculateOffsets().
float _USS_dTof_absTof_offset_results_::dToFOffset |
Contains the averaged DToF computation if USS_calculateOffsets API return USS_message_code_no_error and USS_dTof_absTof_offset_test_config.isCalculateDToFOffset is set to true
Referenced by USS_calculateOffsets().