MSP430UltrasonicLibrary
02_20_00_16
|
Contains USS SW Lib Capture Configuration. More...
#include <ussSwLib.h>
Data Fields | |
USS_Capture_Over_Sample_Rate | overSampleRate |
uint16_t | sampleSize |
USS_Capture_Gain_Range | gainRange |
Configures the internal gain amplifier. More... | |
bool | enableWindowHiComp |
true = enables Window Comparator, false = disables Window Comparator More... | |
bool | enableWindowLoComp |
true = enables Window Comparator, false = disables Window Comparator More... | |
int16_t | windowHighThreshold |
int16_t | windowLowThreshold |
uint16_t | agcConstant |
int16_t * | pCapturesBuffer |
then numberOfAcquisitions = 4. More... | |
uint16_t | maxCapture |
Specifies the maximum capture size. More... | |
bool | isCapAccumulationEnabled |
int16_t * | pAccCaptureBuffer |
(sampleSize*numberOfAcquisitions * 2) bytes and 32 bit aligned. More... | |
Contains USS SW Lib Capture Configuration.
USS_Capture_Over_Sample_Rate _USS_Capture_Configuration_::overSampleRate |
Specifies the oversampling SDHS sample rate. This configuration in combination with pllOutputFreq determines the signal sampling frequency.
Referenced by USS_updateSDHSConfiguration().
uint16_t _USS_Capture_Configuration_::sampleSize |
valid range (1-1024) Configure number of SDHS samples to capture per acquisition sequence.
For example, if acquisition sequence selected is " USS_measurement_capture_sequence_ch0_ch1 " then a total of 2*sampleSize SDHS samples will be captured at the end of the acquisition sequence. If acquisition sequence selected is " USS_measurement_capture_sequence_ch0_ch1_ch0 " then a total of 3*sampleSize SDHS samples will be captured at the end of the acquisition sequence.
Referenced by commonValidateSDHSconfigruation(), USS_calibrateSignalGain(), USS_estimateDCoffset(), and USS_updateSDHSConfiguration().
USS_Capture_Gain_Range _USS_Capture_Configuration_::gainRange |
Configures the internal gain amplifier.
Referenced by USS_calibrateSignalGain(), and USS_updateSDHSConfiguration().
bool _USS_Capture_Configuration_::enableWindowHiComp |
true = enables Window Comparator, false = disables Window Comparator
Referenced by commonDisableCaptureInterrupts(), commonIsconversionSuccessfull(), commonValidateSDHSconfigruation(), and USS_updateSDHSConfiguration().
bool _USS_Capture_Configuration_::enableWindowLoComp |
true = enables Window Comparator, false = disables Window Comparator
Referenced by commonDisableCaptureInterrupts(), commonIsconversionSuccessfull(), commonValidateSDHSconfigruation(), and USS_updateSDHSConfiguration().
int16_t _USS_Capture_Configuration_::windowHighThreshold |
valid range (-2048 to 2047) if enableWindowComp == true, window comparator high threshold is set to user selected value. Otherwise, threshold values keep default reset register value.
Referenced by commonValidateSDHSconfigruation(), and USS_updateSDHSConfiguration().
int16_t _USS_Capture_Configuration_::windowLowThreshold |
valid range (-2048 to 2047) if enableWindowComp == true, window comparator low threshold is set to user selected value. Otherwise, threshold values keep default reset register value.
Referenced by commonValidateSDHSconfigruation(), and USS_updateSDHSConfiguration().
uint16_t _USS_Capture_Configuration_::agcConstant |
This value is use to calculate the Optimal Gain Amplifier setting this value can be determined with the following formula agcConstant = floor(20*log10(adcNom))=floor(20*log10(ADCmax * 10^(-B/20))) where ADCmax = +/- 2^(12-1) for a 12 Bit ADC B = number of db that the ADC output should be backoff (typically 3 db) For USS module for B = 3, agcConstant = floor(20*log10((2^11)*(10^(-3/20)))) = 63
Referenced by USS_calibrateSignalGain().
int16_t* _USS_Capture_Configuration_::pCapturesBuffer |
then numberOfAcquisitions = 4.
Pointer to reserved LEA memory block. Reserved memory block should have a minimum size (sampleSize*numberOfAcquisitions + filterLength * 2) bytes and 32 bit aligned.
If USS_measurement_capture_sequence == USS_measurement_capture_sequence_ch0 then numberOfAcquisitions = 1.
If USS_measurement_capture_sequence == USS_measurement_capture_sequence_chx_chx then numberOfAcquisitions = 2.
If USS_measurement_capture_sequence == USS_measurement_capture_sequence_chx_chx_chx then numberOfAcquisitions = 3.
If USS_measurement_capture_sequence == USS_measurement_capture_sequence_chx_chx_chx_chx
Referenced by commonSDHSRestoreSDHSDTCA().
uint16_t _USS_Capture_Configuration_::maxCapture |
Specifies the maximum capture size.
Referenced by commonValidateSDHSconfigruation().
bool _USS_Capture_Configuration_::isCapAccumulationEnabled |
Pointer to LEA RAM were the sample will be accumulated. Number of accumulations is by dtofVolInterval in Algorithm configuration structure
int16_t* _USS_Capture_Configuration_::pAccCaptureBuffer |
(sampleSize*numberOfAcquisitions * 2) bytes and 32 bit aligned.
Pointer to reserved LEA memory block to perform capture accumulation. Reserved memory block should have a minimum size