SMBus control register. More...
#include <smbus.h>
Data Fields | |
struct { | |
uint8_t pecEn: 1 | |
uint8_t swackEn: 1 | |
Enables PEC functionality. | |
uint8_t intEn: 1 | |
SW_ACK is enabled (read only) | |
uint8_t phyEn: 1 | |
Interupts are enabled (read only) | |
uint8_t master: 1 | |
SMBus PHY is enabled (read only) | |
uint8_t reserved2: 3 | |
Acting in Master mode (read only) | |
} | bits |
Defines the control bit fields. | |
struct { | |
uint8_t writeBits: 1 | |
uint8_t reserved: 7 | |
Control bits that are writable. | |
} | writeableBits |
Allows access to the writeable bits on the structure. | |
uint8_t | u8byte |
Whole Control byte access. | |
SMBus control register.