Definition of SMBus Network structure. More...
#include <smbus.h>
Data Fields | |
volatile SMBus_NwkState | eState |
uint8_t | currentAddr |
Network state machine. | |
uint8_t | currentCmd |
Current Address+R/W. | |
uint8_t | rxIndex |
Current Command. | |
uint8_t | rxLen |
RX Byte counter. | |
uint8_t | rxSize |
Bytes to receive. | |
uint8_t * | rxBuffPtr |
Max size of buffer. | |
uint8_t | txIndex |
Reception Buffer pointer. | |
uint8_t | txLen |
Byte counter. | |
uint8_t * | txBuffPtr |
Bytes to send. | |
uint8_t * | recByteTxPtr |
Transmission pointer. | |
uint8_t | txSize |
Receive Byte response. | |
uint8_t | pec |
Max size of buffer. | |
Definition of SMBus Network structure.