CapTIvate Design Center 1_00_20_00
Release Notes
Document Revision: 102015.1256
This document is divided into the following sections:
What's New
1_00_20_00
- This is the initial release.
Revision_History
No revision history. This is the first release of CapTIvate Design Center.
Stand alone installation
- Download CapTIvate
- Run the appropriate platform specific installer: CapTIvateDesignCenter-<version>-<platform>-installer
- Follow the installer directions
- To launch tool, use the desktop icon or execute the tool directly:
- Windows:
- Start Menu -> All Programs -> Texas Instruments -> CapTIvateDesignCenter_<version> -> CapTIvateDesignCenter
- C:/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter.exe
- OS X
- /Applications/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Linux OS
- ~/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
Device Support
The following families of devices are supported in this release of CapTIvate Design Center :
- MSP430FR2532, MSP430FR2533, MSP430FR2632, MSP430FR2633
CapTIvate Design Center:
- Supported Operating Systems:
- Windows 7
- Apple OS X
- Linux OS
- Java 1.6 or later. Click here to go to Java Download Page.
- Full project generated by CapTIvate Design Center:
- Code Composer Studio (CCS) v6.1.0
- IAR Embedded Workbench 6.30.1
This release is an ES version.
This is build 1_00_20_00 of CapTIvate Design Center.
Additional Resources
For more information, visit www.ti.com.