Build date: 06292016
MSP432 Driver Library is a collection of high level APIs that speed up software development for MSP432. The MSP432 Driver Library package includes API documentaion and examples to help you get started.
This release of MSP432 Driver Library supports all of the following device families:
MSP432 Driver Library is available as a standalone BSD released package. To use the library simply download and unzip the package below. Please read the included user's guide to learn about adding driver library to a new or existing project.
MSP432 Driver Library is also released as a component of MSP432Ware. You can import and run examples from driver library from the TI Resouce Explorer GUI within the Code Composer Studio (CCS) window when you have MSP432Ware installed. For more information about MSP432Ware check the table below for a link to the latest version.
What is the difference between MSP432Ware and Driver Library?MSP432Ware is a collection of MSP432 software and tools. One of the main components of MSP432Ware is Driver Library (DriverLib).
Why are there multiple driverlib folders within MSP432Ware?MSP432Ware contains many different software libraries and projects. Some of these components depend on a specific version of Driver Library. Each component ships the version of Driver Library they tested with to ensure that all software works for you out of the box.
Can I have multiple versions of MSP432Ware installed?Yes! MSP432Ware installations can exist alongside each other. You should only see the latest installed version within the TI Resource Explorer window of Code Composer Studio however.
How can I get support for MSP432Ware?Feel free to use the TI E2E forum to ask anything MSP432Ware related.
Title | Description | Size | |
---|---|---|---|
msp432_driverlib_3_21_00_05.zip | BSD Licensed Driver Library | 10392K | |
Code Composer Studio | Recommended CCS Download | ||
MSP432Ware | Recommended MSP432Ware Download | ||
MSP430 Driver Library | BSD Licensed Driver Library for MSP430 | ||
MSP432 Driver Library Documentation | |||
MSP432 Driver Library Release Notes | |||
MSP432 Driver Library MSP432P4xx | |||
MSP432 Driver Library MSP432P4xx API Guide | |||
MSP432 Driver Library MSP432P4xx Users Guide | 888K | ||
md5sum.txt | MD5 Checksums | 4K |
Fill in Form. Approved users receive download URL in 1 minute.
Fill in Form. TI will contact you in 1-2+ business days.