Go to the source code of this file.
Data Structures | |
struct | _eUSCI_SPI_MasterConfig |
Type definition for _eUSCI_SPI_MasterConfig structure. More... | |
struct | _eUSCI_SPI_SlaveConfig |
Type definition for _eUSCI_SPI_SlaveConfig structure. More... | |
Typedefs | |
typedef struct _eUSCI_SPI_MasterConfig | eUSCI_SPI_MasterConfig |
typedef struct _eUSCI_SPI_SlaveConfig | eUSCI_SPI_SlaveConfig |
Functions | |
bool | SPI_initMaster (uint32_t moduleInstance, const eUSCI_SPI_MasterConfig *config) |
void | SPI_selectFourPinFunctionality (uint32_t moduleInstance, uint_fast8_t select4PinFunctionality) |
void | SPI_changeMasterClock (uint32_t moduleInstance, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
bool | SPI_initSlave (uint32_t moduleInstance, const eUSCI_SPI_SlaveConfig *config) |
void | SPI_changeClockPhasePolarity (uint32_t moduleInstance, uint_fast16_t clockPhase, uint_fast16_t clockPolarity) |
void | SPI_transmitData (uint32_t moduleInstance, uint_fast8_t transmitData) |
uint8_t | SPI_receiveData (uint32_t moduleInstance) |
void | SPI_enableModule (uint32_t moduleInstance) |
void | SPI_disableModule (uint32_t moduleInstance) |
uint32_t | SPI_getReceiveBufferAddressForDMA (uint32_t moduleInstance) |
uint32_t | SPI_getTransmitBufferAddressForDMA (uint32_t moduleInstance) |
uint_fast8_t | SPI_isBusy (uint32_t moduleInstance) |
void | SPI_enableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
void | SPI_disableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
uint_fast8_t | SPI_getInterruptStatus (uint32_t moduleInstance, uint16_t mask) |
uint_fast8_t | SPI_getEnabledInterruptStatus (uint32_t moduleInstance) |
void | SPI_clearInterruptFlag (uint32_t moduleInstance, uint_fast8_t mask) |
void | SPI_registerInterrupt (uint32_t moduleInstance, void(*intHandler)(void)) |
void | SPI_unregisterInterrupt (uint32_t moduleInstance) |
void | EUSCI_A_SPI_select4PinFunctionality (uint32_t baseAddress, uint8_t select4PinFunctionality) |
Selects 4Pin Functionality. More... | |
void | EUSCI_A_SPI_masterChangeClock (uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled. More... | |
bool | EUSCI_A_SPI_slaveInit (uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode) |
Initializes the SPI Slave block. More... | |
void | EUSCI_A_SPI_changeClockPhasePolarity (uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity) |
Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabled. More... | |
void | EUSCI_A_SPI_transmitData (uint32_t baseAddress, uint8_t transmitData) |
Transmits a byte from the SPI Module. More... | |
uint8_t | EUSCI_A_SPI_receiveData (uint32_t baseAddress) |
Receives a byte that has been sent to the SPI Module. More... | |
void | EUSCI_A_SPI_enableInterrupt (uint32_t baseAddress, uint8_t mask) |
Enables individual SPI interrupt sources. More... | |
void | EUSCI_A_SPI_disableInterrupt (uint32_t baseAddress, uint8_t mask) |
Disables individual SPI interrupt sources. More... | |
uint8_t | EUSCI_A_SPI_getInterruptStatus (uint32_t baseAddress, uint8_t mask) |
Gets the current SPI interrupt status. More... | |
void | EUSCI_A_SPI_clearInterruptFlag (uint32_t baseAddress, uint8_t mask) |
Clears the selected SPI interrupt status flag. More... | |
void | EUSCI_A_SPI_enable (uint32_t baseAddress) |
Enables the SPI block. More... | |
void | EUSCI_A_SPI_disable (uint32_t baseAddress) |
Disables the SPI block. More... | |
uint32_t | EUSCI_A_SPI_getReceiveBufferAddressForDMA (uint32_t baseAddress) |
Returns the address of the RX Buffer of the SPI for the DMA module. More... | |
uint32_t | EUSCI_A_SPI_getTransmitBufferAddressForDMA (uint32_t baseAddress) |
Returns the address of the TX Buffer of the SPI for the DMA module. More... | |
bool | EUSCI_A_SPI_isBusy (uint32_t baseAddress) |
Indicates whether or not the SPI bus is busy. More... | |
void | EUSCI_B_SPI_select4PinFunctionality (uint32_t baseAddress, uint8_t select4PinFunctionality) |
Selects 4Pin Functionality. More... | |
void | EUSCI_B_SPI_masterChangeClock (uint32_t baseAddress, uint32_t clockSourceFrequency, uint32_t desiredSpiClock) |
Initializes the SPI Master clock. At the end of this function call, SPI module is left enabled. More... | |
bool | EUSCI_B_SPI_slaveInit (uint32_t baseAddress, uint16_t msbFirst, uint16_t clockPhase, uint16_t clockPolarity, uint16_t spiMode) |
Initializes the SPI Slave block. More... | |
void | EUSCI_B_SPI_changeClockPhasePolarity (uint32_t baseAddress, uint16_t clockPhase, uint16_t clockPolarity) |
Changes the SPI colock phase and polarity. At the end of this function call, SPI module is left enabled. More... | |
void | EUSCI_B_SPI_transmitData (uint32_t baseAddress, uint8_t transmitData) |
Transmits a byte from the SPI Module. More... | |
uint8_t | EUSCI_B_SPI_receiveData (uint32_t baseAddress) |
Receives a byte that has been sent to the SPI Module. More... | |
void | EUSCI_B_SPI_enableInterrupt (uint32_t baseAddress, uint8_t mask) |
Enables individual SPI interrupt sources. More... | |
void | EUSCI_B_SPI_disableInterrupt (uint32_t baseAddress, uint8_t mask) |
Disables individual SPI interrupt sources. More... | |
uint8_t | EUSCI_B_SPI_getInterruptStatus (uint32_t baseAddress, uint8_t mask) |
Gets the current SPI interrupt status. More... | |
void | EUSCI_B_SPI_clearInterruptFlag (uint32_t baseAddress, uint8_t mask) |
Clears the selected SPI interrupt status flag. More... | |
void | EUSCI_B_SPI_enable (uint32_t baseAddress) |
Enables the SPI block. More... | |
void | EUSCI_B_SPI_disable (uint32_t baseAddress) |
Disables the SPI block. More... | |
uint32_t | EUSCI_B_SPI_getReceiveBufferAddressForDMA (uint32_t baseAddress) |
Returns the address of the RX Buffer of the SPI for the DMA module. More... | |
uint32_t | EUSCI_B_SPI_getTransmitBufferAddressForDMA (uint32_t baseAddress) |
Returns the address of the TX Buffer of the SPI for the DMA module. More... | |
bool | EUSCI_B_SPI_isBusy (uint32_t baseAddress) |
Indicates whether or not the SPI bus is busy. More... | |