MSP430 DriverLib for MSP430FR2xx_4xx Devices  2.91.03.00
 All Data Structures Functions Variables Groups Pages
MSP430 DriverLib for MSP430FR2xx_4xx Devices

Introduction

This package provides API documentation for all the peripherals in the MSP430 Driver Library. MSP430 Driver Library provides an easy to use API for developing applications for the MSP430FR2xx_4xx devices.

The easiest way to get started is to click on the "Modules" tab above. This will provide an alphabetical list of peripherals available in the MSP430 Driver Library.

This API documentation is broken out into the following sections:

  • Documentation Tab
    • List of modules contained within this family of Driver Library
  • Data Structures Tab
    • Data Structures, a list of data structures defined by Driver Library
    • Data Fields, a list of fields available in the data structures
  • Files Tab
    • File List, an alphabetical list of peripheral API's available in MSP430 Driver Library
    • Globals, an alphabetical list of MSP430 Driver Library global definitions

Also note the existence of the following content available on disk. This is not part of this API but contains useful example code and documentation.

  • Example Code
    • under examples/driverlib/MSP430FR2xx_4xx/{peripheral}
  • Users Guide
    • doc/driverlib/MSP430FR2xx_4xx/MSP430FR2xx_4xx_DriverLib_Users_Guide-2.91.03.00.pdf

Copyright 2017, Texas Instruments Incorporated