Functions for performing forward and inverse FFT of real 16-bit and 32-bit input data.
Real forward FFT function with auto-scaling.
- Details
- Computes the forward discreet Fourier transform (DFT) of 16-bit real inputs. If the inputs are not already in bit reversed order the bit reversal parameter must be set. The output is monitored for overflow and scaled by a factor of two when an overflow risk is detected. The shift parameter contains the number of bit shifts that were applied to the output.
- This functions requires half the data storage and consumes roughly half the cycles and energy as running a complex FFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = fft(real(x)) * 2^-shift
- Scaling
- Scaling is applied as needed to prevent saturation of the output. The scale factor that was applied to the output is returned in the shift parameter and can be used to calculate the result by applying the following function.
result = result * 2^shift
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to twice the data length (e.g. a 256-point real FFT requires 512-byte alignment). When allocating data the MSP_ALIGN_FFT_Q15 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
shift | Auto-scaling shift that was applied to the output. |
- Returns
- Status of the operation.
Real forward FFT function with fixed scaling by two at each stage.
- Details
- Computes the forward discreet Fourier transform (DFT) of 16-bit real inputs. If the inputs are not already in bit reversed order the bit reversal parameter must be set. The output is scaled by a factor of two for each stage of the DFT.
- This functions requires half the data storage and consumes roughly half the cycles and energy as running a complex FFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = fft(real(x)) ./ (N/2)
- Scaling
- Each stage of the real FFT, with the exception of the final split stage, scales the result by a factor of 0.5. The output format can either be interpreted as the same type with (N/2) scaling or a different fixed point data type. This can be helpful when using the IQmathLib to process the results of the FFT, such as computing the magnitude or phase angle of the complex result.
-
Length | Input Type | Result Type |
16 | _q15 | _q12 |
32 | _q15 | _q11 |
64 | _q15 | _q10 |
128 | _q15 | _q9 |
256 | _q15 | _q8 |
512 | _q15 | _q7 |
1024 | _q15 | _q6 |
2048 | _q15 | _q5 |
4096 | _q15 | _q4 |
- The following table lists the applied scaling factor and resulting data type when the input is a 16-bit integer.
-
Length | Input Type | Result Type |
16 | int16_t | (int16_t)(result / 8) |
32 | int16_t | (int16_t)(result / 16) |
64 | int16_t | (int16_t)(result / 32) |
128 | int16_t | (int16_t)(result / 64) |
256 | int16_t | (int16_t)(result / 128) |
512 | int16_t | (int16_t)(result / 256) |
1024 | int16_t | (int16_t)(result / 512) |
2048 | int16_t | (int16_t)(result / 1024) |
4096 | int16_t | (int16_t)(result / 2048) |
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to twice the data length (e.g. a 256-point real FFT requires 512-byte alignment). When allocating data the MSP_ALIGN_FFT_Q15 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
- Returns
- Status of the operation.
- Examples:
- transform_ex1_fft_fixed_q15.c.
Real forward FFT function without scaling.
- Details
- Computes the forward discreet Fourier transform (DFT) of 32-bit real inputs. If the inputs are not already in bit reversed order the bit reversal parameter must be set. The output is not scaled.
- This functions requires half the data storage and consumes roughly half the cycles and energy as running a complex FFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = fft(real(x))
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to four times the data length (e.g. a 256-point real FFT requires 1024-byte alignment). When allocating data the MSP_ALIGN_FFT_IQ31 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
- Returns
- Status of the operation.
- Examples:
- transform_ex3_fft_iq31.c.
Real result inverse FFT function with auto-scaling.
- Details
- Computes the inverse discreet Fourier transform (DFT) of 16-bit complex inputs with real result. If the inputs are not already in bit reversed order the bit reversal parameter must be set. Automatic scaling is performed such that this is the direct inverse of the forward FFT with auto scaling.
- This functions uses half the data storage and consumes roughly half the cycles and energy as running a complex IFFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = (real(ifft(x)) * 2^shift) ./ (N/2)
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to twice the data length (e.g. a 256-point real FFT requires 512-byte alignment). When allocating data the MSP_ALIGN_FFT_Q15 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
shift | Auto-scaling shift that was applied to the forward FFT. |
- Returns
- Status of the operation.
Real result inverse FFT function with fixed scaling by two at each stage.
- Details
- Computes the inverse discreet Fourier transform (DFT) of 16-bit complex inputs with real result. If the inputs are not already in bit reversed order the bit reversal parameter must be set. Fixed scaling is performed such that this is the direct inverse of the forward FFT with fixed scaling.
- This functions uses half the data storage and consumes roughly half the cycles and energy as running a complex IFFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = real(ifft(x))
- Scaling
- This function is the direct inverse of the forward real FFT with fixed scaling. The following fixed point input types will all result in Q15 results.
-
Length | Input Type | Result Type |
16 | _q12 | _q15 |
32 | _q11 | _q15 |
64 | _q10 | _q15 |
128 | _q9 | _q15 |
256 | _q8 | _q15 |
512 | _q7 | _q15 |
1024 | _q6 | _q15 |
2048 | _q5 | _q15 |
4096 | _q4 | _q15 |
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to twice the data length (e.g. a 256-point real FFT requires 512-byte alignment). When allocating data the MSP_ALIGN_FFT_Q15 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
- Returns
- Status of the operation.
Real result inverse FFT function without scaling.
- Details
- Computes the inverse discreet Fourier transform (DFT) of 32-bit complex inputs with real result. If the inputs are not already in bit reversed order the bit reversal parameter must be set. Fixed scaling is performed such that this is the direct inverse of the forward FFT without scaling.
- This functions uses half the data storage and consumes roughly half the cycles and energy as running a complex IFFT of the same length. When transforming purely real inputs, such as samples from an ADC or analog sensor, it is recommended to use the real FFT functions.
- Pseudo code
y = real(ifft(x)) ./ N
- LEA Support
- This function is supported by LEA and requires data to be placed into shared LEA memory with alignment equal to four times the data length (e.g. a 256-point real FFT requires 1024-byte alignment). When allocating data the MSP_ALIGN_FFT_IQ31 macro can be used to calculate correct alignment. The twiddle table pointer parameter is not used with LEA and can be null or uninitialized.
- Parameters
-
params | Pointer to the real FFT parameter structure. |
src | Pointer to the real data array to perform the FFT on. |
- Returns
- Status of the operation.