Texas Instruments

MSP430Ware 3.60.00.10

Table of Contents

Introduction

This is 3.60.00.10 of MSP430Ware. MSP430Ware will allow you to develop your applications faster by providing all MSP430 related examples, documentation and software libraries in one package.

Documentation

Software Libraries

Folder Description Documentation
driverlib MSP430 Driver Library Release Notes
usblib430 MSP430 USB Developer’s Package Release Notes
grlib MSP430 Graphics Library Release Notes
fram_utilities FRAM Utilities Release Notes
iec60740 MSP430 IEC60740 Software Package Release Notes
captouchlib Capacitive Touch Software Library Readme
captivate CapTIvate Design Center and Software Library Release Notes
iqmathlib IQmath Library Release Notes
dsplib DSP Library Release Notes
smbuslib SMBus Library Release Notes
pmbuslib PMBus Library Release Notes
nfclink NFCLink NFC/HF RFID Firmware Library Readme

Development Tool Support

Folder Description Hardware Documentation Software Documentation
examples/boards/MSP-EXP430F5529LP MSP-EXP430F5529LP Readme Readme
examples/boards/MSP-EXP430FR4133 MSP-EXP430FR4133 Readme Readme
examples/boards/MSP-EXP430G2 MSP-EXP430G2 Readme Readme
examples/boards/MSP-EXP430FR5969 MSP-EXP430FR5969 Readme Readme
examples/boards/MSP-EXP430FR6989 MSP-EXP430FR6989 Readme Readme
examples/boards/MSP-EXP430FR5739 MSP-EXP430FR5739 Readme Readme
examples/boards/MSP-EXP430F5529 MSP-EXP430F5529 Readme Readme
examples/boards/MSP-CAPT-FR2633 MSP-CAPT-FR2633 Readme CapTIvate Design Center and Software Library Release Notes
examples/boards/MSP-EXP430FR2311 MSP-EXP430FR2311 Readme Readme
examples/boards/MSP-EXP430FR5994 MSP-EXP430FR5994 Readme Readme
examples/boards/MSP-EXP430F5438 MSP-EXP430F5438 Not included in MSPWare Readme
examples/boards/430BOOST-SENSE1 430BOOST-SENSE1 Readme N/A
examples/boards/430BOOST-SHARP96 430BOOST-SHARP96 Readme N/A
examples/boards/BOOST-IR BOOST-IR Readme N/A
examples/boards/BOOSTXL-EDUMKII BOOSTXL-EDUMKII Readme N/A
examples/boards/BOOSTXL-K350QVG-S1 BOOSTXL-K350QVG-S1 Readme N/A
examples/boards/BOOSTXL-AUDIO BOOSTXL-AUDIO Readme N/A
examples/boards/MSP-ISO MSP-ISO Readme N/A
examples/boards/EVM430-FR6989 EVM430-FR6989 Readme Readme

Tools

Folder Description Documentation
touchpro TouchPro GUI Release Notes
flowesi Flow ESI GUI Release Notes
msp_flasher MSP Flasher README

Other Documentation

What’s New

3.60.00.10

Revision History

3.50.00.04

3.40.00.19

3.30.00.18

3.20.00.37

2.40.00.37

2.30.00.49

2.21.00.39

2.20.00.19

2.10.00.15

2.00.00.41

1.97.00.47

1.95.00.32

1.90.00.30

1.80.01.03

1.80.00.17

1.70.00.28

1.60.03.07

1.60.02.09

1.60.01.11

1.60.00.38

1.40.01.44

1.40.01.19

1.40.00.26

1.30.00.15

1.25.00.30

Upgrade and Compatibility Information

MSP430Ware 3.60.00.10 may be installed along any previous version of MSP430Ware. It will place a new directory in “C:\ti\msp\MSP430Ware_3_60_00_10” on Windows and a similar location on Linux and Mac OS X. The older version will still be available on disk but CCS will discover and use the latest for TI Resource Explorer.

Installation and Usage

There are two methods to install MSP430Ware:

Installing via the Code Composer Studio (CCS) App Center

  1. If you have CCS 6.0 or later you can install MSP430Ware via the CCS App Center.
  2. Open up CCS
  3. Click “View->CCS App Center”
  4. Click the checkbox next to MSP430Ware
  5. Then click “Install Software” in the top left corner of the app center.
  6. Let CCS restart and discover the software. You can now use TI Resource Explorer within CCS

Installing via the Standalone Installer

If CCS is not your primary IDE or want an offline installer on hand you can download the standalone installer.

  1. Download the standalone installer for your operating system from the MSP430Ware download page.
  2. Double click to run the installer, the default installation path is discoverable by CCS
  3. Run CCS and let it discover the MSP430Ware installation. You can now use TI Resource Explorer within CCS

Host Support

Supported Operating Systems:

Some components are not supported on all platforms. Check out the Known Issues part of the release notes for more information about what is not supported in each operating system.

Dependencies

This release requires the following other software components and tools versions to successfully function:

Please look at the individual packages release notes to see their dependencies.

Device Support

Please look at the individual packages release notes to determine what devices they support. For MSP432 device support please check out MSP432Ware.

Validation Information

This is a GA release of MSP430Ware. Please check the individual packages release notes to determine their validation information. If you encounter bugs with this release please contact us at .

Known Issues

MSP430Ware is a collection of different packages from Texas Instruments. Some packages have not been updated to support Linux or Mac OS X Yosemite. A list of known packages that are not updated can be seen below. Please check the release notes of the individual packages for more information.

Linux Support

Mac OS X Yosemite Support

Versioning

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. MSP430Ware_3_40_00_10.

Technical Support and Product Updates

Additional Resources

For more information about Texas Instruments, MSP430 or MSP432 visit www.ti.com and www.msp430.com.