CapTIvate Design Center 1.30.10.00
Table of Contents
This is version 1.30.10.00 of the CapTIvate Design Center.
Brief description of what the product does.
Note: Change these links to match the installation directory structure for your product.
- Updated to CapTIvate Software Library v1.04.00.00
- Added support for using the VLO to clock the CapTIvate timer in LPM4 when in wake-on-proximity mode to the CAPT_App layer. This allows applications to achieve very low average power consumption when a crystal is not used for the low frequency clock (ACLK). Entering LPM4 disables ACLK (turning of XT1 or the REFO, whichever was used for ACLK). The CapTIvate peripheral may still be clocked from the VLO in LPM4, if the VLO is selected as the clock source. The trade-off with using this mode is reduced time-keeping accuracy in wake-on-proximity mode. To enable this feature, define CAPT_WOP_VLO_LPM4 in CAPT_App.c. For more details, see the Ultra Low Power section of the Design Guide chapter of the CapTIvate Technology Guide.
- Added the ProximityRangeSensor example project. This example project shows how to implement a basic range sensing application using the CAPTIVATE-PROXIMITY sensing panel.
- The MSP peripheral driver library is updated to include support for the DCO manual trim procedure.
- The CapTIvate Starter Project default stack size was reduced to 256B from 512B. Testing estimates the worst case stack usage for most applications to be <128B.
- Documentation updates
- v1.20.00.00
- Documentation updates
- Minor bug fixes
- v1.10.00.00
- Documentation updates
- Fix intermittent GUI startup issues
- Other minor bug fixes
- v1.00.20.00
- Initial public ES release
- Download CapTIvate
- Run the appropriate platform specific installer: CapTIvateDesignCenter---installer
- Follow the installer directions
- To launch tool, use the desktop icon or execute the tool directly:
- Windows
- Start Menu -> All Programs -> Texas Instruments -> CapTIvateDesignCenter_<version> -> CapTIvateDesignCenter
- C:/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter.exe
- OS X
- /Applications/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
- Linux OS
- ~/ti/msp/CapTIvateDesignCenter_<version>/CapTIvateDesignCenter
Supported Operating Systems:
- Windows 7
- Linux OS
- Apple OS X
The following families of devices are supported in this release of CapTIvate Design Center:
- MSP430FR2532, MSP430FR2533
- MSP430FR2632, MSP430FR2633
This is a production RTM release.
No known issues currently.
This is build 1.30.10.00 of CapTIvate Design Center
For more information about Texas Instruments, MSP430 or MSP432 visit www.ti.com and www.msp430.com.