Data Fields
_HAL_ADC_SD24_B_Configuration_ Struct Reference

Contains the SD24 Configuration. More...

#include <hal_adc_sd24b.h>

Collaboration diagram for _HAL_ADC_SD24_B_Configuration_:
Collaboration graph
[legend]

Data Fields

uint32_t SMCLKFrequency
 Sub-System Clock (SMCLK) Frequency in Hz. More...
 
uint16_t overSampleRatio
 
uint16_t sampleFreq
 
SD24_B_initParam * sd24Param
 
uint8_t masterConverter
 Pointer to struct for SD24_B initialization. More...
 
HAL_ADC_SD24_B_ChanneladcChannelPtr
 The highest converter used to start / stop conversions. More...
 
uint8_t adcChannelLength
 Pointer to the location where the channel configuration is stored. More...
 

Detailed Description

Contains the SD24 Configuration.

Field Documentation

§ SMCLKFrequency

uint32_t _HAL_ADC_SD24_B_Configuration_::SMCLKFrequency

Sub-System Clock (SMCLK) Frequency in Hz.

§ overSampleRatio

uint16_t _HAL_ADC_SD24_B_Configuration_::overSampleRatio

§ sampleFreq

uint16_t _HAL_ADC_SD24_B_Configuration_::sampleFreq

Selects oversampling ratio for the converter
Valid values are:

  • SD24_B_OVERSAMPLE_32
  • SD24_B_OVERSAMPLE_64
  • SD24_B_OVERSAMPLE_128
  • SD24_B_OVERSAMPLE_256
  • SD24_B_OVERSAMPLE_1024 Sample Frequency for each converter
    Valid values are:
  • HAL_ADC_FREQ_2048_HZ
  • HAL_ADC_FREQ_4096_HZ
  • HAL_ADC_FREQ_8192_HZ
  • HAL_ADC_FREQ_16384_HZ

§ sd24Param

SD24_B_initParam* _HAL_ADC_SD24_B_Configuration_::sd24Param

§ masterConverter

uint8_t _HAL_ADC_SD24_B_Configuration_::masterConverter

Pointer to struct for SD24_B initialization.

§ adcChannelPtr

HAL_ADC_SD24_B_Channel* _HAL_ADC_SD24_B_Configuration_::adcChannelPtr

The highest converter used to start / stop conversions.

§ adcChannelLength

uint8_t _HAL_ADC_SD24_B_Configuration_::adcChannelLength

Pointer to the location where the channel configuration is stored.


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale