Contains the SD24 Channel Configuration. More...
#include <hal_adc_sd24.h>
Data Fields | |
uint8_t | gain |
uint8_t | preload |
Preload of the Sigma Delta 24 Channel- Valid 0x00 to SD24_MAX_PRELOAD. More... | |
int32_t * | samplePtr |
Channel enabled used to initialize the SD24 channel. More... | |
uint8_t | converter |
Contains the SD24 Channel Configuration.
uint8_t _HAL_ADC_SD24_Channel_::gain |
Gain of the Sigma Delta 24 channel Valid values are:
uint8_t _HAL_ADC_SD24_Channel_::preload |
Preload of the Sigma Delta 24 Channel- Valid 0x00 to SD24_MAX_PRELOAD.
int32_t* _HAL_ADC_SD24_Channel_::samplePtr |
Channel enabled used to initialize the SD24 channel.
uint8_t _HAL_ADC_SD24_Channel_::converter |