Contains the SD24 Configuration. More...
#include <hal_adc_sd24b.h>
Data Fields | |
uint32_t | SMCLKFrequency |
Sub-System Clock (SMCLK) Frequency in Hz. More... | |
uint16_t | overSampleRatio |
uint16_t | sampleFreq |
SD24_B_initParam * | sd24Param |
uint8_t | masterConverter |
Pointer to struct for SD24_B initialization. More... | |
HAL_ADC_SD24_B_Channel * | adcChannelPtr |
The highest converter used to start / stop conversions. More... | |
uint8_t | adcChannelLength |
Pointer to the location where the channel configuration is stored. More... | |
Contains the SD24 Configuration.
uint32_t _HAL_ADC_SD24_B_Configuration_::SMCLKFrequency |
Sub-System Clock (SMCLK) Frequency in Hz.
uint16_t _HAL_ADC_SD24_B_Configuration_::overSampleRatio |
uint16_t _HAL_ADC_SD24_B_Configuration_::sampleFreq |
Selects oversampling ratio for the converter
Valid values are:
SD24_B_initParam* _HAL_ADC_SD24_B_Configuration_::sd24Param |
uint8_t _HAL_ADC_SD24_B_Configuration_::masterConverter |
Pointer to struct for SD24_B initialization.
HAL_ADC_SD24_B_Channel* _HAL_ADC_SD24_B_Configuration_::adcChannelPtr |
The highest converter used to start / stop conversions.
uint8_t _HAL_ADC_SD24_B_Configuration_::adcChannelLength |
Pointer to the location where the channel configuration is stored.