Contains the SD24 Channel Configuration. More...
#include <hal_adc_sd24b.h>
Data Fields | |
uint8_t | gain |
uint16_t | preload |
Preload of the Sigma Delta 24 Channel. More... | |
uint8_t | converter |
uint8_t | alignment |
Contains the SD24 Channel Configuration.
uint8_t _HAL_ADC_SD24_B_Channel_::gain |
Gain of the Sigma Delta 24 channel Valid values are:
uint16_t _HAL_ADC_SD24_B_Channel_::preload |
Preload of the Sigma Delta 24 Channel.
uint8_t _HAL_ADC_SD24_B_Channel_::converter |
uint8_t _HAL_ADC_SD24_B_Channel_::alignment |
Selects the converter that will be configured. Check datasheet for available converters on device.
Valid values are: