Data Fields
_EM_Meter_Configuration_ Struct Reference

Contains EM SW Lib Meter Configuration. More...

#include <emSwLib.h>

Collaboration diagram for _EM_Meter_Configuration_:
Collaboration graph
[legend]

Data Fields

EM_Phase_ConfigurationphaseConfigPtr
 Pointer to the EM_Phase_Configuration struct buffer. More...
 
uint8_t phaseLength
 Length of the emPhasePtr buffer. More...
 
uint8_t * meterName
 Pointer to meter name string. More...
 
uint8_t * libVersionNumber
 Pointer to library version number string. More...
 
uint8_t * meterPW
 

Detailed Description

Contains EM SW Lib Meter Configuration.

Field Documentation

§ phaseConfigPtr

EM_Phase_Configuration* _EM_Meter_Configuration_::phaseConfigPtr

Pointer to the EM_Phase_Configuration struct buffer.

§ phaseLength

uint8_t _EM_Meter_Configuration_::phaseLength

Length of the emPhasePtr buffer.

§ meterName

uint8_t* _EM_Meter_Configuration_::meterName

Pointer to meter name string.

§ libVersionNumber

uint8_t* _EM_Meter_Configuration_::libVersionNumber

Pointer to library version number string.

§ meterPW

uint8_t* _EM_Meter_Configuration_::meterPW

The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated