Data Fields
_EM_Algorithm_Configuration_ Struct Reference

Contains EM SW Lib Algorithm Configuration. More...

#include <emSwLib.h>

Data Fields

EM_Power_t residualPowerCutoff
 
EM_Power_t totalResidualPowerCutoff
 
uint8_t mainNomFreq
 Nominal Freq value for the system (Hz) More...
 
_iq29 sqrtTwoConst
 Square of 2 constant used for Vpeak and Ipeak calculations. More...
 
_iq30 energyCalcConst
 One dividing by (3600 x sampling frequency) More...
 
uint16_t freqSampling
 Sampling Frequency (Hz) More...
 
uint16_t reactPowIIRMinFreq
 Min Frequency for the IIR coefficient table. More...
 
uint8_t reactPowIIRShift
 Number of shifts required to calculated index for IIR table. More...
 
uint16_t reactPowIIRLength
 Length of the IIR coefficient table. More...
 
_iq30 * reactPowIIRTable
 

Detailed Description

Contains EM SW Lib Algorithm Configuration.

Field Documentation

§ residualPowerCutoff

EM_Power_t _EM_Algorithm_Configuration_::residualPowerCutoff

Residual Power Cutoff per each phase. This threshold is used as the minimum value of power to store. Power values below this value will not be stored.

§ totalResidualPowerCutoff

EM_Power_t _EM_Algorithm_Configuration_::totalResidualPowerCutoff

Residual Power Cutoff for the sum of all the phases. If the sum of all phase power values is below this value, the total power value will not be updated.

§ mainNomFreq

uint8_t _EM_Algorithm_Configuration_::mainNomFreq

Nominal Freq value for the system (Hz)

§ sqrtTwoConst

_iq29 _EM_Algorithm_Configuration_::sqrtTwoConst

Square of 2 constant used for Vpeak and Ipeak calculations.

§ energyCalcConst

_iq30 _EM_Algorithm_Configuration_::energyCalcConst

One dividing by (3600 x sampling frequency)

§ freqSampling

uint16_t _EM_Algorithm_Configuration_::freqSampling

Sampling Frequency (Hz)

§ reactPowIIRMinFreq

uint16_t _EM_Algorithm_Configuration_::reactPowIIRMinFreq

Min Frequency for the IIR coefficient table.

§ reactPowIIRShift

uint8_t _EM_Algorithm_Configuration_::reactPowIIRShift

Number of shifts required to calculated index for IIR table.

§ reactPowIIRLength

uint16_t _EM_Algorithm_Configuration_::reactPowIIRLength

Length of the IIR coefficient table.

§ reactPowIIRTable

_iq30* _EM_Algorithm_Configuration_::reactPowIIRTable

The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated