Logo
MSP DSP Library
msp_interleave_q15_params Struct Reference

Parameters for Q15 vector interleave. More...

#include <DSPLib_utility.h>

Data Fields

uint16_t length
 Length of each channel, must be a multiple of two.
 
uint16_t channel
 Specific zero-indexed channel to insert source into.
 
uint16_t numChannels
 Number of channels in destination vector.
 

Detailed Description

Parameters for Q15 vector interleave.


The documentation for this struct was generated from the following file: