Logo
MSP DSP Library
MSP_LEA_IIRBQ1_PARAMS Struct Reference

Parameter structure for LEACMD__IIRBQ1 command. More...

#include <DSPLib_lea.h>

Data Fields

uint16_t vectorSizeBy2
 Length of data vector divided by two.
 
uint16_t output
 Output data vector.
 
uint16_t state
 Biquad state structure.
 
uint16_t coeffs
 Biquad coefficient structure.
 
uint16_t direction
 Input increment direction.
 
uint16_t reserved
 Reserved padding.
 

Detailed Description

Parameter structure for LEACMD__IIRBQ1 command.


The documentation for this struct was generated from the following file: