Logo
MSP DSP Library
MSP_LEA_FFTLONG_PARAMS Struct Reference

Parameter structure for LEACMD__FFTLONG command. More...

#include <DSPLib_lea.h>

Data Fields

uint16_t vectorSize
 Length of data vector,must be a power of two.
 
uint16_t log2Size
 Log base 2 of vectorSize parameter.
 

Detailed Description

Parameter structure for LEACMD__FFTLONG command.


The documentation for this struct was generated from the following file: