1 #ifndef __DSPLIB_FILTER_H__
2 #define __DSPLIB_FILTER_H__
45 #define MSP_ALIGN_FIR_Q15(n) (n*4)
55 #define MSP_ALIGN_FIR_IQ31(n) (n*8)
65 #define MSP_ALIGN_CMPLX_FIR_Q15(n) (n*8)
75 #define MSP_ALIGN_CMPLX_FIR_IQ31(n) (n*16)
831 #endif //__DSPLIB_FILTER_H__
msp_biquad_df1_q15_states * states
Definition: DSPLib_filter.h:262
_q15 q2
Definition: DSPLib_filter.h:313
uint16_t length
Definition: DSPLib_filter.h:153
uint16_t length
Definition: DSPLib_filter.h:326
_q15 min
Definition: DSPLib_filter.h:432
uint16_t length
Definition: DSPLib_filter.h:248
msp_biquad_df2_ext_q15_states * states
Definition: DSPLib_filter.h:458
Coefficients for direct form 2 biquad filter. When using LEA these coefficients must be placed into s...
Definition: DSPLib_filter.h:273
_q15 x2
Definition: DSPLib_filter.h:203
States for direct form 1 biquad filter.
Definition: DSPLib_filter.h:200
int32_t _iq31
Signed fixed point data type with 1 integer bit and 31 fractional bits.
Definition: DSPLib_types.h:100
uint16_t reserved1
Definition: DSPLib_filter.h:184
_q15 b1By2
Definition: DSPLib_filter.h:395
_q15 b2
Definition: DSPLib_filter.h:294
uint16_t length
Definition: DSPLib_filter.h:448
_q15 y2
Definition: DSPLib_filter.h:209
const _q15 * coeffs
Definition: DSPLib_filter.h:93
Parameter structure for FIR filter.
Definition: DSPLib_filter.h:106
uint16_t reserved1
Definition: DSPLib_filter.h:276
_q15 b2
Definition: DSPLib_filter.h:175
uint16_t tapLength
Definition: DSPLib_filter.h:90
msp_status
Enumerated type to return the status of an operation.
Definition: DSPLib_types.h:119
msp_biquad_df2_ext_q15_states * states
Definition: DSPLib_filter.h:486
uint16_t tapLength
Definition: DSPLib_filter.h:134
uint16_t length
Definition: DSPLib_filter.h:109
_q15 q1
Definition: DSPLib_filter.h:310
Parameter structure for direct form 1 biquad filter.
Definition: DSPLib_filter.h:222
Coefficients for extended direct form 2 biquad filter. When using LEA these coefficients must be plac...
Definition: DSPLib_filter.h:374
_q15 a1By2
Definition: DSPLib_filter.h:386
bool enableCircularBuffer
Definition: DSPLib_filter.h:140
msp_biquad_df2_q15_states * states
Definition: DSPLib_filter.h:336
msp_status msp_cmplx_fir_iq31(const msp_cmplx_fir_iq31_params *params, const _iq31 *src, _iq31 *dst)
Discrete-time convolution of a complex source vector with complex coefficients to apply an FIR filter...
Parameter structure for cascaded direct form 2 biquad filter.
Definition: DSPLib_filter.h:346
const _iq31 * coeffs
Definition: DSPLib_filter.h:115
_q15 b0
Definition: DSPLib_filter.h:392
_q15 a1By2
Definition: DSPLib_filter.h:282
bool enableCircularBuffer
Definition: DSPLib_filter.h:96
const _iq31 * coeffs
Definition: DSPLib_filter.h:159
Parameter structure for extended direct form 2 biquad filter.
Definition: DSPLib_filter.h:445
_q15 b2
Definition: DSPLib_filter.h:398
const msp_biquad_df2_ext_q15_coeffs * coeffs
Definition: DSPLib_filter.h:480
_q15 b1By2
Definition: DSPLib_filter.h:178
const msp_biquad_df1_q15_coeffs * coeffs
Definition: DSPLib_filter.h:256
msp_status msp_biquad_df2_q15(const msp_biquad_df2_q15_params *params, const _q15 *src, _q15 *dst)
Second-order direct form 2 biquad filter.
uint16_t stages
Definition: DSPLib_filter.h:353
msp_biquad_df1_q15_states * states
Definition: DSPLib_filter.h:235
_q15 a0
Definition: DSPLib_filter.h:389
_q15 b1By2
Definition: DSPLib_filter.h:291
msp_status msp_biquad_df1_q15(const msp_biquad_df1_q15_params *params, const _q15 *src, _q15 *dst)
Second-order direct form 1 biquad filter.
_q15 a1By2
Definition: DSPLib_filter.h:190
_iq31 bias
Definition: DSPLib_filter.h:377
msp_status msp_biquad_df2_ext_q15(const msp_biquad_df2_ext_q15_params *params, const _q15 *src, _q15 *dst)
Second-order direct form 2 biquad filter extended with DC bias and minimum and maximum tracking...
_q15 b0
Definition: DSPLib_filter.h:181
States for extended direct form 2 biquad filter.
Definition: DSPLib_filter.h:411
uint16_t stages
Definition: DSPLib_filter.h:476
_q15 a2
Definition: DSPLib_filter.h:187
_q15 minOdd
Definition: DSPLib_filter.h:423
Coefficients for direct form 1 biquad filter.
Definition: DSPLib_filter.h:172
States for direct form 2 biquad filter.
Definition: DSPLib_filter.h:307
Parameter structure for FIR filter.
Definition: DSPLib_filter.h:84
uint16_t stages
Definition: DSPLib_filter.h:252
uint16_t length
Definition: DSPLib_filter.h:131
_q15 q1
Definition: DSPLib_filter.h:414
_q15 a0
Definition: DSPLib_filter.h:285
int16_t _q15
Signed fixed point data type with 1 integer bit and 15 fractional bits.
Definition: DSPLib_types.h:79
const _q15 * coeffs
Definition: DSPLib_filter.h:137
uint16_t length
Definition: DSPLib_filter.h:472
const msp_biquad_df2_q15_coeffs * coeffs
Definition: DSPLib_filter.h:330
msp_status msp_biquad_cascade_df2_ext_q15(const msp_biquad_cascade_df2_ext_q15_params *params, const _q15 *src, _q15 *dst)
Cascaded direct form 2 biquad filter extended with DC bias and minimum and maximum tracking...
Parameter structure for cascaded extended direct form 2 biquad filter.
Definition: DSPLib_filter.h:469
_q15 y1
Definition: DSPLib_filter.h:212
msp_status msp_fir_q15(const msp_fir_q15_params *params, const _q15 *src, _q15 *dst)
Discrete-time convolution of a source vector with real coefficients to apply an FIR filter...
_q15 max
Definition: DSPLib_filter.h:435
msp_status msp_cmplx_fir_q15(const msp_cmplx_fir_q15_params *params, const _q15 *src, _q15 *dst)
Discrete-time convolution of a complex source vector with complex coefficients to apply an FIR filter...
bool enableCircularBuffer
Definition: DSPLib_filter.h:118
uint16_t reserved2
Definition: DSPLib_filter.h:297
_q15 q2
Definition: DSPLib_filter.h:417
Parameter structure for complex FIR filter.
Definition: DSPLib_filter.h:128
msp_status msp_biquad_cascade_df2_q15(const msp_biquad_cascade_df2_q15_params *params, const _q15 *src, _q15 *dst)
Cascaded direct form 2 biquad filter.
_q15 maxOdd
Definition: DSPLib_filter.h:429
const msp_biquad_df1_q15_coeffs * coeffs
Definition: DSPLib_filter.h:229
_q15 maxEven
Definition: DSPLib_filter.h:426
_q15 a2
Definition: DSPLib_filter.h:383
_q15 x1
Definition: DSPLib_filter.h:206
Parameter structure for direct form 2 biquad filter.
Definition: DSPLib_filter.h:323
_q15 a2
Definition: DSPLib_filter.h:279
uint16_t tapLength
Definition: DSPLib_filter.h:112
msp_biquad_df2_q15_states * states
Definition: DSPLib_filter.h:363
uint16_t tapLength
Definition: DSPLib_filter.h:156
Parameter structure for complex FIR filter.
Definition: DSPLib_filter.h:150
const msp_biquad_df2_ext_q15_coeffs * coeffs
Definition: DSPLib_filter.h:452
uint16_t length
Definition: DSPLib_filter.h:225
Parameter structure for cascaded direct form 1 biquad filter.
Definition: DSPLib_filter.h:245
uint16_t length
Definition: DSPLib_filter.h:349
uint16_t reserved1
Definition: DSPLib_filter.h:380
_q15 minEven
Definition: DSPLib_filter.h:420
_q15 b0
Definition: DSPLib_filter.h:288
msp_status msp_biquad_cascade_df1_q15(const msp_biquad_cascade_df1_q15_params *params, const _q15 *src, _q15 *dst)
Cascaded direct form 1 biquad filter.
uint16_t reserved2
Definition: DSPLib_filter.h:401
msp_status msp_fir_iq31(const msp_fir_iq31_params *params, const _iq31 *src, _iq31 *dst)
Discrete-time convolution of a source vector with real coefficients to apply an FIR filter...
uint16_t length
Definition: DSPLib_filter.h:87
bool enableCircularBuffer
Definition: DSPLib_filter.h:162
const msp_biquad_df2_q15_coeffs * coeffs
Definition: DSPLib_filter.h:357