MSP430™CapTIvateSoftwareLibraryAPIGuide  1_83_00_05
Data Fields
tDeBounceSettings Struct Reference

typedef tDeBounceSettings More...

#include <CAPT_Type.h>

Data Fields

uint8_t DbIn: 4
 
uint8_t DbOut: 4
 

Detailed Description

typedef tDeBounceSettings

The de-bounce structure holds de-bounce up/down information, and can be used for storing de-bounce thresholds or counts.

Field Documentation

§ DbIn

uint8_t tDeBounceSettings::DbIn

De-bounce into a Touch/Prox State May hold the threshold or the current de-bounce count

§ DbOut

uint8_t tDeBounceSettings::DbOut

De-bounce out of a Touch/Prox State May hold the threshold or the current de-bounce count


The documentation for this struct was generated from the following file:
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale