TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
gattClientCharCfgUpdatedEvent_t Struct Reference

GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format. More...

Data Fields

uint16 attrHandle
 attribute handle
 
uint16 connHandle
 Connection message was received on.
 
osal_event_hdr_t hdr
 GATT_SERV_MSG_EVENT and status.
 
uint8 method
 GATT_CLIENT_CHAR_CFG_UPDATED_EVENT.
 
uint16 value
 attribute new value
 

Detailed Description

GATT_CLIENT_CHAR_CFG_UPDATED_EVENT message format.

This message is sent to the app when a Client Characteristic Configuration is updated.


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated