TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
gapPairingReq_t Struct Reference

Data Fields

uint8_t authReq
 Pairing Request Auth Req field.
 
uint8_t ioCap
 Pairing Request ioCap field.
 
keyDist_t keyDist
 Pairing Request Key Distribution field.
 
uint8_t maxEncKeySize
 Pairing Request Maximum Encryption Key Size field.
 
uint8_t oobDataFlag
 Pairing Request OOB Data Flag field.
 

Detailed Description

Pairing Request fields for GAP_Authenticate which should only be used if the gapbondmgr does not exist


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated