TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
GapAdv_truncData_t Struct Reference

Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event. More...

Data Fields

uint16 advDataLen
 
uint8 availAdvDataLen
 How many bytes of the advertising data were sent.
 
uint8 handle
 Advertising handle.
 

Detailed Description

Data type returned with GAP_EVT_ADV_DATA_TRUNCATED event.

Field Documentation

§ advDataLen

uint16 advDataLen

Total length of the advertising data that was attempted to send


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated