TI BLE5-Stack API Documentation
1.01.01.00
|
TRNG driver implementation for a CC26XX device. More...
Modules | |
TRNG_STATUS | |
Files | |
file | TRNGCC26XX.h |
TRNG driver implementation for a CC26XX device. | |
Data Structures | |
struct | TRNGCC26XX_Config |
TRNGCC26XX Global Configuration. More... | |
struct | TRNGCC26XX_HWAttrs |
TRNGCC26XX Hardware Attributes. More... | |
struct | TRNGCC26XX_Object |
TRNGCC26XX Object. More... | |
struct | TRNGCC26XX_Params |
TRNGCC26XX Parameters. More... | |
Macros | |
#define | TRNGCC26XX_CLOCKS_PER_SAMPLES_MAX 15 |
#define | TRNGCC26XX_ILLEGAL_PARAM_RETURN_VALUE 0 |
#define | TRNGCC26XX_MAX_SAMPLES_MAX 16777216 |
#define | TRNGCC26XX_MAX_SAMPLES_MIN 256 |
#define | TRNGCC26XX_MIN_SAMPLES_MAX 16384 |
#define | TRNGCC26XX_MIN_SAMPLES_MIN 64 |
Typedefs | |
typedef struct TRNGCC26XX_Config | TRNGCC26XX_Config |
TRNGCC26XX Global Configuration. | |
typedef struct TRNGCC26XX_Config * | TRNGCC26XX_Handle |
A handle that is returned from a TRNGCC26XX_open() call. | |
typedef struct TRNGCC26XX_HWAttrs | TRNGCC26XX_HWAttrs |
TRNGCC26XX Hardware Attributes. More... | |
typedef struct TRNGCC26XX_Object | TRNGCC26XX_Object |
TRNGCC26XX Object. More... | |
typedef struct TRNGCC26XX_Params | TRNGCC26XX_Params |
TRNGCC26XX Parameters. More... | |
Functions | |
void | TRNGCC26XX_close (TRNGCC26XX_Handle handle) |
Close the TRNG driver. More... | |
uint32_t | TRNGCC26XX_getNumber (TRNGCC26XX_Handle handle, TRNGCC26XX_Params *params, int8_t *status) |
This routine returns a 32 bit TRNG number. More... | |
void | TRNGCC26XX_init (void) |
TRNG Driver initialization. More... | |
int8_t | TRNGCC26XX_isParamValid (TRNGCC26XX_Params *params) |
Check that the parameters used are valid configurations. More... | |
TRNGCC26XX_Handle | TRNGCC26XX_open (uint8_t index) |
Open the TRNGCC26XX peripheral specified by the index value. This peripheral will be configured as specified by pParams. Alternatively, if pParams is NULL, default values will be used. More... | |
int8_t | TRNGCC26XX_Params_init (TRNGCC26XX_Params *params) |
Initialize TRNG configuration parameters to their defaults. More... | |
TRNG driver implementation for a CC26XX device.
============================================================================
The TRNG header file should be included in an application as follows:
The TRNGCC26XX driver provides reentrant access to the TRNG module within the CC26XX. Reentrant access is controlled by creating a global critical section when requesting a random number. This critical section disables all Hwi's from running.
For code examples, see the use cases below.
If an error occurs during a call to TRNGCC26XX_getNumber, the error status will be set into the status flag and the returned random number shall be 0. passing the status flag is optional.
API function | Description |
---|---|
TRNGCC26XX_open() | Open driver (stub) |
TRNGCC26XX_close() | Close driver (stub) |
TRNGCC26XX_Params_init() | Initialize parameters for random number generation |
TRNGCC26XX_init() | Generates a random number |
TRNGCC26XX_isParamValid | Validate client configuration parameters |
#define TRNGCC26XX_CLOCKS_PER_SAMPLES_MAX 15 |
Number of clocks cycles per sample must be between 1 (0) and 16 (15), inclusive.
#define TRNGCC26XX_ILLEGAL_PARAM_RETURN_VALUE 0 |
Number returned from TRNGCC26XX_getNumber when invalid parameters are used.
#define TRNGCC26XX_MAX_SAMPLES_MAX 16777216 |
Maximum samples per cycle range, maximum value
Maximum may be 0, or greater than or equal to 2^8 and less than or equal to 2^24.
#define TRNGCC26XX_MAX_SAMPLES_MIN 256 |
Maximum samples per cycle range, minimum value
Maximum may be 0, or greater than or equal to 2^8 and less than or equal to 2^24.
#define TRNGCC26XX_MIN_SAMPLES_MAX 16384 |
Minimum samples per cycle range, maximum value
Minimum may be 0, or greater than or equal to 2^6 and less than 2^14.
#define TRNGCC26XX_MIN_SAMPLES_MIN 64 |
Minimum samples per cycle range, minimum value
Minimum may be 0, or greater than or equal to 2^6 and less than 2^14.
typedef struct TRNGCC26XX_HWAttrs TRNGCC26XX_HWAttrs |
TRNGCC26XX Hardware Attributes.
Hardware Attribute structure for TRNG peripherals.
typedef struct TRNGCC26XX_Object TRNGCC26XX_Object |
TRNGCC26XX Object.
The application must not access any member variables of this structure!
typedef struct TRNGCC26XX_Params TRNGCC26XX_Params |
TRNGCC26XX Parameters.
This holds the TRNG configuration parameters to be used. see the functions description of TRNGConfigure() in trng.h for more information.
void TRNGCC26XX_close | ( | TRNGCC26XX_Handle | handle | ) |
Close the TRNG driver.
handle | a TRNGCC26XX_Handle returned from TRNGCC26XX_open(). |
uint32_t TRNGCC26XX_getNumber | ( | TRNGCC26XX_Handle | handle, |
TRNGCC26XX_Params * | params, | ||
int8_t * | status | ||
) |
This routine returns a 32 bit TRNG number.
params | - caller's configuration parameters. input parameter. |
status | - a user provided pointer to a status flag in case of failure. This parameter may be left NULL. output parameter. TRNGCC26XX_STATUS_SUCCESS if successful. TRNGCC26XX_STATUS_ILLEGAL_PARAM if params is null or configuration is illegal. |
handle | a TRNGCC26XX_Handle returned from TRNGCC26XX_open |
void TRNGCC26XX_init | ( | void | ) |
TRNG Driver initialization.
int8_t TRNGCC26XX_isParamValid | ( | TRNGCC26XX_Params * | params | ) |
Check that the parameters used are valid configurations.
params | - caller's configuration parameters. input parameter. |
TRNGCC26XX_Handle TRNGCC26XX_open | ( | uint8_t | index | ) |
Open the TRNGCC26XX peripheral specified by the index value. This peripheral will be configured as specified by pParams. Alternatively, if pParams is NULL, default values will be used.
index | Logical peripheral Number indexed in the HWAttrs table. |
int8_t TRNGCC26XX_Params_init | ( | TRNGCC26XX_Params * | params | ) |
Initialize TRNG configuration parameters to their defaults.
params | - TRNG configuration parameters. input parameter. |