|
#define | RF_EventCmdDone (1<<0) |
| Radio operation command finished. More...
|
|
#define | RF_EventLastCmdDone (1<<1) |
| Last radio operation command in a chain finished. More...
|
|
#define | RF_EventFGCmdDone (1<<2) |
| Last radio operation command in a chain finished. More...
|
|
#define | RF_EventLastFGCmdDone (1<<3) |
| Last radio operation command in a chain finished. More...
|
|
#define | RF_EventTxDone (1<<4) |
| Packet transmitted. More...
|
|
#define | RF_EventTXAck (1<<5) |
| ACK packet transmitted. More...
|
|
#define | RF_EventTxCtrl (1<<6) |
| Control packet transmitted. More...
|
|
#define | RF_EventTxCtrlAck (1<<7) |
| Acknowledgement received on a transmitted control packet. More...
|
|
#define | RF_EventTxCtrlAckAck (1<<8) |
| Acknowledgement received on a transmitted control packet, and acknowledgement transmitted for that packet. More...
|
|
#define | RF_EventTxRetrans (1<<9) |
| Packet retransmitted. More...
|
|
#define | RF_EventTxEntryDone (1<<10) |
| Tx queue data entry state changed to Finished. More...
|
|
#define | RF_EventTxBufferChange (1<<11) |
| A buffer change is complete. More...
|
|
#define | RF_EventRxOk (1<<16) |
| Packet received with CRC OK, payload, and not to be ignored. More...
|
|
#define | RF_EventRxNOk (1<<17) |
| Packet received with CRC error. More...
|
|
#define | RF_EventRxIgnored (1<<18) |
| Packet received with CRC OK, but to be ignored. More...
|
|
#define | RF_EventRxEmpty (1<<19) |
| Packet received with CRC OK, not to be ignored, no payload. More...
|
|
#define | RF_EventRxCtrl (1<<20) |
| Control packet received with CRC OK, not to be ignored. More...
|
|
#define | RF_EventRxCtrlAck (1<<21) |
| Control packet received with CRC OK, not to be ignored, then ACK sent. More...
|
|
#define | RF_EventRxBufFull (1<<22) |
| Packet received that did not fit in the Rx queue. More...
|
|
#define | RF_EventRxEntryDone (1<<23) |
| Rx queue data entry changing state to Finished. More...
|
|
#define | RF_EventDataWritten (1<<24) |
| Data written to partial read Rx buffer. More...
|
|
#define | RF_EventNDataWritten (1<<25) |
| Specified number of bytes written to partial read Rx buffer. More...
|
|
#define | RF_EventRxAborted (1<<26) |
| Packet reception stopped before packet was done. More...
|
|
#define | RF_EventRxCollisionDetected (1<<27) |
| A collision was indicated during packet reception. More...
|
|
#define | RF_EventModulesUnlocked (1<<29) |
| As part of the boot process, the CM0 has opened access to RF core modules and memories. More...
|
|
#define | RF_EventInternalError (uint32_t)(1<<31) |
| Internal error observed. More...
|
|
#define | RF_EventMdmSoft 0x0000002000000000 |
| Modem Sync detected (MDMSOFT IFG) More...
|
|