BLE-Stack APIs
1.00.00
|
Parameter Structure for the Connection terminated Event. More...
Data Fields | |
uint16_t | connHandle |
2 Byte Handle of the connection | |
uint8_t | reason |
1 Byte Reason of the termination connection termination reason. | |
Parameter Structure for the Connection terminated Event.
See SNP Event Indication for more information.
This is a packed structure. see Dealing with Parameters and Packed Structures for more information.