![]() |
![]() |
BLE-Stack APIs
3.00.00
|
![]() ![]() | ATT layer interface |
![]() ![]() | Type definitions and macros for BLE stack |
![]() ![]() | Central layer interface |
![]() ![]() | Common Defines |
![]() ![]() | GAP layer interface |
![]() ![]() | GAPBondMgr layer interface |
![]() ![]() | GATT layer interface |
![]() ![]() | GATTServApp layer interface |
![]() ![]() | HCI layer interface |
![]() ![]() | Types, constants, external functions etc. for the BLE HCI Transport Layer |
![]() ![]() | ICall layer interface |
![]() ![]() | Stack image address information specific to build |
![]() ![]() | Indirect function Call dispatcher constant definitions specific to CC26xx platform |
![]() ![]() | L2CAP layer interface |
![]() ![]() | LinkDB layer interface |
![]() ![]() | Multi layer interface |
![]() ![]() | This API allows the software components in the Z-Stack to be written independently of the specifics of the operating system, kernel, or tasking environment (including control loops or connect-to-interrupt systems) |
![]() ![]() | Peripheral layer interface |
![]() ![]() | This file contains the interface to the SM |
![]() ![]() | This file contains the interface to the Micro Link Layer |
![]() ![]() | Micro BLE GAP API |
![]() ![]() | This file contains configurable variables for the Micro BLE Stack radio |
![]() ![]() | Util layer interface |