TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpUpdateConnParamReq_t Struct Reference

Parameter Structure for SNP_updateConnParam. More...

Data Fields

uint16_t connHandle
 2 Byte handle of the connection to update parameters to.
 
uint16_t intervalMax
 2 Byte Maximum value for the connection event interval. More...
 
uint16_t intervalMin
 2 Byte Minimum value for the connection event interval. More...
 
uint16_t slaveLatency
 2 Byte Slave latency for the connection in number of connection events. More...
 
uint16_t supervisionTimeout
 2 Byte Supervision timeout for the LE Link. More...
 

Detailed Description

Parameter Structure for SNP_updateConnParam.

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.

Field Documentation

§ intervalMax

uint16_t intervalMax

2 Byte Maximum value for the connection event interval.

This shall be greater than or equal to intervalMin.
Range: 0x0006 to 0x0C80
Time = intervalMax * 1.25 msec
Time Range: 7.5 msec to 4 seconds.

§ intervalMin

uint16_t intervalMin

2 Byte Minimum value for the connection event interval.

This shall be less than or equal to intervalMax.
Range: 0x0006 to 0x0C80
Time = intervalMin * 1.25 msec
Time Range: 7.5 msec to 4 seconds.

§ slaveLatency

uint16_t slaveLatency

2 Byte Slave latency for the connection in number of connection events.

Range: 0x0000 to 0x01F3

§ supervisionTimeout

uint16_t supervisionTimeout

2 Byte Supervision timeout for the LE Link.

Range: 0x000A to 0x0C80
Time = connTimeout * 10 msec
Time Range: 100 msec to 32 seconds


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated