TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
linkDBItem_t Struct Reference

linkDB item More...

Data Fields

uint8 addr [B_ADDR_LEN]
 Other Device's address.
 
uint8 addrPriv [B_ADDR_LEN]
 Other Device's Private address.
 
uint8 addrType
 Address type of connected device.
 
uint16 connectionHandle
 Controller connection handle.
 
uint16 connInterval
 The connection's interval (n * 1.23 ms)
 
uint8 connRole
 Connection formed as Master or Slave.
 
uint16 MTU
 The connection's MTU size.
 
encParams_tpEncParams
 pointer to LTK, ediv, rand. if needed.
 
linkSec_t sec
 Connection Security related items.
 
uint8 stateFlags
 LINK_CONNECTED, LINK_AUTHENTICATED...
 
uint8 taskID
 Application that controls the link.
 

Detailed Description

linkDB item


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated