TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
hciRetParam_LeReadBufSize_t Struct Reference

Data structure for HCI Command Complete Event Return Parameter. More...

Data Fields

uint16 dataPktLen
 data packet length
 
uint8 numDataPkts
 number of data packets
 
uint8 status
 status of event
 

Detailed Description

Data structure for HCI Command Complete Event Return Parameter.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated