TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
snpGetGapParamRsp_t Struct Reference

Parameter Structure for the Get GAP Parameter Value Response. More...

Data Fields

uint16_t paramId
 2 Byte GAP Parameter ID, GAP Parameter IDs
 
uint8_t status
 1 Byte Status of the request (SUCCESS or Error, list of status generated by the SNP.)
 
uint16_t value
 2 Byte Parameter Value retrieved.
 

Detailed Description

Parameter Structure for the Get GAP Parameter Value Response.

Used for SNP_GET_GAP_PARAM_RSP

This is a packed structure. see Dealing with Parameters and Packed Structures for more information.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated