TI BLE-Stack for Bluetooth 4.2 API Documentation  3.01.00.07
Data Fields
attPacket_t Struct Reference

Attribute Protocol PDU format. More...

Data Fields

uint8 cmd
 Command Flag.
 
uint16 len
 Length of Attribute Parameters.
 
uint8 method
 Method.
 
uint8 * pParams
 Attribute Parameters.
 
uint8 sig
 Authentication Signature status (not included (0), valid (1), invalid (2))
 

Detailed Description

Attribute Protocol PDU format.


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated