TI BLE5-Stack API Documentation  1.01.01.00
Data Fields
hciEvt_BLEReadRemoteFeatureComplete_t Struct Reference

LE Read Remote Used Features Complete Event. More...

Data Fields

uint8 BLEEventCode
 BLE Event Code.
 
uint16 connectionHandle
 connection handle
 
uint8 features [8]
 features
 
osal_event_hdr_t hdr
 osal event header
 
uint8 status
 status of event
 

Detailed Description

LE Read Remote Used Features Complete Event.


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated