TIOVX User Guide
|
Structure describing a shared memory pointer. More...
#include <tivx_mem.h>
Data Fields | |
volatile uint32_t | mem_heap_region |
Memory region to which this pointer belongs, see tivx_mem_heap_region_e. | |
volatile int32_t | dma_buf_fd |
Value of dmaBufFd corresponds to the host_ptr, This will be used by host/Linux CPU. | |
volatile uint64_t | shared_ptr |
Value of pointer as seen in shared memory All CPUs will have method to convert from shared memory pointer to CPU local memory pointer. | |
volatile uint64_t | host_ptr |
Value of pointer as seen as by host CPU Host CPU will have method to convert to/from shared memory pointer. | |
volatile uint32_t | dma_buf_fd_offset |
Offset of dmaBufFd, This will be used by host/Linux CPU. | |
Structure describing a shared memory pointer.
Definition at line 188 of file tivx_mem.h.