TIOVX User Guide

TIDL params structure. More...

#include <j7_tidl.h>

Data Fields

vx_uint8 config_checksum [TIVX_TIDL_J7_CHECKSUM_SIZE]
 
vx_uint8 network_checksum [TIVX_TIDL_J7_CHECKSUM_SIZE]
 
vx_uint32 compute_config_checksum
 
vx_uint32 compute_network_checksum
 
sTIDL_IOBufDesc_t ioBufDesc
 
vx_uint32 optimize_ivision_activation
 

Detailed Description

TIDL params structure.

Definition at line 97 of file j7_tidl.h.

Field Documentation

◆ config_checksum

vx_uint8 tivxTIDLJ7Params::config_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE]

Checksum placeholder for TIDL config params

Definition at line 99 of file j7_tidl.h.

◆ network_checksum

vx_uint8 tivxTIDLJ7Params::network_checksum[TIVX_TIDL_J7_CHECKSUM_SIZE]

Checksum placeholder for TIDL network params

Definition at line 102 of file j7_tidl.h.

◆ compute_config_checksum

vx_uint32 tivxTIDLJ7Params::compute_config_checksum

Flag to indicate if config params checksum is to be computed or not

Definition at line 105 of file j7_tidl.h.

◆ compute_network_checksum

vx_uint32 tivxTIDLJ7Params::compute_network_checksum

Flag to indicate if network params checksum is to be computed or not

Definition at line 108 of file j7_tidl.h.

◆ ioBufDesc

sTIDL_IOBufDesc_t tivxTIDLJ7Params::ioBufDesc

TIDL input/output buffer descriptor

Definition at line 111 of file j7_tidl.h.

◆ optimize_ivision_activation

vx_uint32 tivxTIDLJ7Params::optimize_ivision_activation

Flag to enable optimization ivision alg activate, default it is disabled

Definition at line 114 of file j7_tidl.h.


The documentation for this struct was generated from the following file: