TIOVX User Guide
tiovx.enums.Target Class Reference

Target on which to execute a node (TIOVX equivalent = TIVX_TARGET_xxxx) More...

Inherits Enum.

Static Public Attributes

int INVALID = 1
 Placeholder for invalid target ID.
 
int DSP1 = 2
 TIOVX equivalent = TIVX_TARGET_DSP1.
 
int DSP2 = 3
 TIOVX equivalent = TIVX_TARGET_DSP2.
 
int EVE1 = 4
 TIOVX equivalent = TIVX_TARGET_EVE1.
 
int EVE2 = 5
 TIOVX equivalent = TIVX_TARGET_EVE2.
 
int EVE3 = 6
 TIOVX equivalent = TIVX_TARGET_EVE3.
 
int EVE4 = 7
 TIOVX equivalent = TIVX_TARGET_EVE4.
 
int A15_0 = 8
 TIOVX equivalent = TIVX_TARGET_A15_0.
 
int MCU2_0 = 9
 TIOVX equivalent = TIVX_TARGET_MCU2_0.
 
int MCU2_1 = 10
 TIOVX equivalent = TIVX_TARGET_MCU2_1.
 
int IPU2 = 11
 TIOVX equivalent = TIVX_TARGET_IPU2.
 
int VPAC_NF = 12
 Below are J7 targets TIOVX equivalent = TIVX_TARGET_VPAC_NF.
 
int VPAC_LDC1 = 13
 TIOVX equivalent = TIVX_TARGET_VPAC_LDC1.
 
int VPAC_LDC2 = 14
 TIOVX equivalent = TIVX_TARGET_VPAC_LDC2.
 
int VPAC_MSC1 = 15
 TIOVX equivalent = TIVX_TARGET_VPAC_MSC1.
 
int VPAC_MSC2 = 16
 TIOVX equivalent = TIVX_TARGET_VPAC_MSC2.
 
int DMPAC_SDE = 17
 TIOVX equivalent = TIVX_TARGET_DMPAC_SDE.
 
int DMPAC_DOF = 18
 TIOVX equivalent = TIVX_TARGET_DMPAC_DOF.
 
int VPAC_VISS1 = 19
 TIOVX equivalent = TIVX_TARGET_VPAC_VISS1.
 
int DSP_C7_1 = 24
 TIOVX equivalent = TIVX_TARGET_DSP_C7_1.
 
int MPU_0 = 25
 TIOVX equivalent = TIVX_TARGET_MPU_0.
 
int DEFAULT = DSP1
 Above are J7 targets Used internally by the tool.
 

Detailed Description

Target on which to execute a node (TIOVX equivalent = TIVX_TARGET_xxxx)

Used as parameter when creating a node

Example usage:
Target.DSP1
Target.DSP2

Definition at line 414 of file enums.py.


The documentation for this class was generated from the following file: