TIOVX User Guide
tiovx.core.Core Class Reference

Core. More...

Inherits Enum.

Static Public Attributes

string C66 = "c66"
 Target is C66.
 
string EVE = "eve"
 Target is EVE.
 
string IPU = "ipu"
 Target is IPU.
 
string A15 = "a15"
 Target is A15.
 
string ARM = "arm"
 Target is an ARM core.
 
string GPU = "gpu"
 Target is a GPU.
 
string VPAC_NF = "vpac_nf"
 Below are J7 cores Target is an VPAC_NF HWA.
 
string DMPAC_SDE = "dmpac_sde"
 Target is an DMPAC_SDE HWA.
 
string VPAC_LDC = "vpac_ldc"
 Target is an VPAC_LDC HWA.
 
string VPAC_MSC = "vpac_msc"
 Target is an VPAC_MSC HWA.
 
string VPAC_VISS = "vpac_viss"
 Target is an VPAC_VISS HWA.
 
string DMPAC_DOF = "dmpac_dof"
 Target is an DMPAC_DOF HWA.
 
string C7X = "c7x"
 Target is a C7X DSP.
 
string MPU = "mpu"
 Target is an MPU.
 

Detailed Description

Core.

Definition at line 67 of file core.py.


The documentation for this class was generated from the following file: