MCUSW
Icu_Cfg.h File Reference

Introduction

This file contains generated pre compile configuration file for ICU MCAL driver.

Go to the source code of this file.

Macros

#define ICU_PRE_COMPILE_VARIANT   (STD_ON )
 ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) More...
 
#define ICU_SAFETY_DIAGNOSTIC_API   (STD_ON)
 Enable/Disable Icu Safety Diagnostic. More...
 
#define ICU_DE_INIT_API   (STD_ON)
 Enable/Disable Icu DeInit API. More...
 
#define ICU_EDGE_COUNT_API   (STD_ON)
 Enable/Disable Edge Count API. More...
 
#define ICU_EDGE_DETECT_API   (STD_ON)
 Enable/Disable Edge Detect API. More...
 
#define ICU_GET_DUTY_CYCLE_VALUES_API   (STD_ON)
 Enable/Disable Get Duty Cycle Values API. More...
 
#define ICU_GET_INPUT_STATE_API   (STD_ON)
 Enable/Disable Get Input State API. More...
 
#define ICU_GET_TIME_ELAPSED_API   (STD_ON)
 Enable/Disable Get Time Elapsed API. More...
 
#define ICU_GET_VERSION_INFO_API   (STD_ON)
 Enable/Disable Get Version Info API. More...
 
#define ICU_SIGNAL_MEASUREMENT_API   (STD_ON)
 Enable/Disable Signal Measurement API. More...
 
#define ICU_TIMESTAMP_API   (STD_ON)
 Enable/Disable Timestamp API. More...
 
#define ICU_DEV_ERROR_DETECT   (STD_ON)
 Enable/Disable Development error detet. More...
 
#define ICU_WAKEUP_FUNCTIONALITY_API   (STD_OFF)
 Enable/disable ICU wakeup functionality API. More...
 
#define ICU_ENABLEWAKEUP_API   (STD_OFF)
 Enable/disable ICU wakeup functionality API. More...
 
#define ICU_DISABLEWAKEUP_API   (STD_OFF)
 Enable/disable ICU wakeup functionality API. More...
 
#define ICU_SETMODE_API   (STD_OFF)
 Enable/Disable Icu set mode API. More...
 
#define IcuConf_IcuChannel_IcuChannel_0   (1U)
 Channel ID Symbolic Names Configured channel ID(s) More...
 
#define ICU_INIT_CONFIG_PC   IcuConfigSet
 Pre Compile config macro name. More...
 
#define ICU_ISR_TYPE   (ICU_ISR_CAT1)
 ISR type. More...
 
#define ICU_MAX_NUM_CHANNELS   (3U)
 
#define ICU_CHANNEL1   (1U)
 ECAP Channel 1, in MAIN DOMAIN. More...
 

Functions

void Icu_ch1Notify (void)
 ICU ISR. More...
 

Variables

const uint32 Icu_HwUnitBaseAddr [ICU_MAX_NUM_CHANNELS]
 
const struct Icu_ConfigType_PC_s IcuConfigSet_PC
 ICU Configuration structure declaration. More...
 
const struct Icu_ConfigType_s IcuConfigSet