ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_LEAVE_VLAN command.
Parameters provided by remote clients to leave a VLAN previously joined using ETHREMOTECFG_CMD_JOIN_VLAN command. After successfully leaving the VLAN, VLAN traffic will stop on the provided RX flow.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint16_t | vlanId |
uint8_t | macAddr [ETHREMOTECFG_MACADDRLEN] |
uint32_t | flowIdxBase |
uint32_t | flowIdxOffset |
EthRemoteCfg_ReqHdr EthRemoteCfg_VlanLeaveReq::hdr |
Request message common header.
uint16_t EthRemoteCfg_VlanLeaveReq::vlanId |
VLAN id.
uint8_t EthRemoteCfg_VlanLeaveReq::macAddr[ETHREMOTECFG_MACADDRLEN] |
MAC address.
uint32_t EthRemoteCfg_VlanLeaveReq::flowIdxBase |
RX flow index base.
uint32_t EthRemoteCfg_VlanLeaveReq::flowIdxOffset |
RX flow index offset to route unicast VLAN packets to.