ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_JOIN_VLAN command.
Parameters provided by remote clients to join a VLAN previously setup by Ethernet Firmware. The remote client must be allowed to join the requested EthRemoteCfg_VlanJoinReq::vlanId for the request to succeed. If allowed, VLAN traffic will be routed to the RX flow provided by the client.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint16_t | vlanId |
uint8_t | macAddr [ETHREMOTECFG_MACADDRLEN] |
uint32_t | flowIdxBase |
uint32_t | flowIdxOffset |
EthRemoteCfg_ReqHdr EthRemoteCfg_VlanJoinReq::hdr |
Request message common header.
uint16_t EthRemoteCfg_VlanJoinReq::vlanId |
VLAN id.
uint8_t EthRemoteCfg_VlanJoinReq::macAddr[ETHREMOTECFG_MACADDRLEN] |
MAC address.
uint32_t EthRemoteCfg_VlanJoinReq::flowIdxBase |
RX flow index base.
uint32_t EthRemoteCfg_VlanJoinReq::flowIdxOffset |
RX flow index offset to route unicast VLAN packets to.