ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_SET_RX_DEFAULTFLOW or ETHREMOTECFG_CMD_DEL_RX_DEFAULTFLOW commands.
This structure holds info about the rxFlowIdx which needs to be registered or de-registred as default flow.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint32_t | flowIdxBase |
uint32_t | flowIdxOffset |
EthRemoteCfg_ReqHdr EthRemoteCfg_RxDefaultFlowRegisterReq::hdr |
Request message common header.
uint32_t EthRemoteCfg_RxDefaultFlowRegisterReq::flowIdxBase |
Rx flow index base.
uint32_t EthRemoteCfg_RxDefaultFlowRegisterReq::flowIdxOffset |
Rx flow index offset