ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_REGISTER_WRITE command.
Request structure holds the address of the register and the value which needs to be written into the register.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint32_t | addr |
uint32_t | val |
EthRemoteCfg_ReqHdr EthRemoteCfg_RegWriteReq::hdr |
Request message common header.
uint32_t EthRemoteCfg_RegWriteReq::addr |
Register address.
uint32_t EthRemoteCfg_RegWriteReq::val |
Value which needs to be written.