ETHFW API Guide
|
Response params for ETHREMOTECFG_CMD_IOCTL command.
This is response structure for EthRemoteCfg_IoctlReq.
Data Fields | |
EthRemoteCfg_ResHdr | hdr |
uint32_t | cmd |
uint32_t | outArgsLen |
uint64_t | outArgs [(ETHREMOTECFG_IOCTL_OUTARGS_LEN/sizeof(uint64_t))] |
EthRemoteCfg_ResHdr EthRemoteCfg_IoctlRes::hdr |
Response message common header.
uint32_t EthRemoteCfg_IoctlRes::cmd |
Enet LLD IOCTL command id. Refer Enet LLD documentation for list of available IOCTLs.
uint32_t EthRemoteCfg_IoctlRes::outArgsLen |
Enet LLD IOCTL command output arguments length.
uint64_t EthRemoteCfg_IoctlRes::outArgs[(ETHREMOTECFG_IOCTL_OUTARGS_LEN/sizeof(uint64_t))] |
Enet LLD IOCTL command output arguments. Byte array is typecast to the outArgs structure associated with the IOCTL.