ETHFW API Guide
|
Request params for ETHREMOTECFG_CMD_DEREGISTER_IPv4 command.
This structure holds IPv4 address which will be used as a key to remove the entry from the proxy ARP table of the server.
Data Fields | |
EthRemoteCfg_ReqHdr | hdr |
uint8_t | ipAddr [ETHREMOTECFG_IPV4ADDRLEN] |
EthRemoteCfg_ReqHdr EthRemoteCfg_IPv4AddrDeregisterReq::hdr |
Request message common header.
uint8_t EthRemoteCfg_IPv4AddrDeregisterReq::ipAddr[ETHREMOTECFG_IPV4ADDRLEN] |
IP address.